Pairing the device with the Wiser Hub
- On the Home screen, tap
Devices.
The Device Management screen appears. - Tap Devices > +.The Add Device screen appears.
- Tap Preferred > With
Hub >
Dual Curtain Controller (A).
- Enter the following Device Information and then tap Next:
-
Enter Device Name: Enter the device name.
-
Assign Existing Room: Select an existing room.
TIP: If your room is not in the existing room list, create a new one. -
Add New Room: Create a new room.
-
- Tap Next and choose one of the following
options to pair the device with the Wiser Hub.
-
Press the pairing button once and make sure that the LED blinks green.
Wait for a few seconds until the LED turns green.
TIP: If the LED is blinking red, then the device is not paired to the Hub. Reset the device and start pairing again. -
Press the toggle Switch-1 3 times (Sequence: ON-OFF ON-OFF ON-OFF) within 4 seconds.
NOTE: If the relay puck is installed inside the wall box, the status LED is not visible.
-
- After a few minutes, you will see the Wiser message. Tap Ok.You can see the newly added device on the Device Management screen under Devices.