DUG_Wiser Curtain Controller-00

Using the device

The Device Control Screen allows you to Open/Close the shutter and control various settings.
  1. On the Home screen, tap Devices > Devices.

  2. Select the device which you want to access the Device Control Screen.

The Device Control Screen displays the following options:

A

Shutter Percentage

Allows you to set the percentage of how much the shutter opens.

B

Shutter Controls

Allow you to open, stop, or close the shutter.

  • Open: To open the shutter.

  • Stop: To stop the shutter at any position.

  • Close: To close the shutter.

C

Schedule

Allows you to create quick actions and trigger automations.

D

History

Allows you to see the history of the device. Tap to update the history of the device when you open the History screen.

E

Settings

Allows you to control various settings. For more information, refer to the Configuring the device topic.

F

Favourites

Allows you to add the device to the favourites on the Home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?