DUG_Wiser Curtain Controller-00

Creating an action

An action allows you to group multiple actions that are usually done together. Using the Wiser app, you can create actions based on your needs (such as movie night).

To create an action:

  1. On the Automations screen, tap Quick.
  2. On the bottom-right screen, tap + to create an action.
    The Add Action screen appears.
  3. Select one of the following options as per your preference:
    • Add a Sequence (A): Switch ON multiple devices in a sequence.

    • Add Quick Action (B): Switch ON multiple devices at a time.

    TIP: Follow the below steps to create an action for both Add a Sequence (A) and Add Quick Action (B). The only difference is that you need to enter the time gap for Add a Sequence.
  4. Tap Add Device (C) and select either a device or an action:
    • Devices (D): Select a device from the list and set the device status (e.g., ON/OFF, delay). Then, tap Done.

    • Control actions (E): Tap View all actions, select an action from the list, and set the action status. Then, tap Save.

    TIP: Tap and enter your device name to find it.
  5. Repeat steps 4 to add more than one device or an action.
    TIP: You can change the waiting time by tapping the time (F) (Only for Add a Sequence).
    NOTE: By default, the time gap is 2 seconds, and the maximum time gap you can select is 120 seconds.
  6. Enter the Action Name (G).
  7. Tap Icon (H) and select the icon from the list.
  8. Tap Notification (J) and enable the toggle button for the following options and then tap Save (L):
    • Show timeline: Displays the total power consumption.

    • Push notifications: Receives the notifications.

    NOTE: To switch the toggle buttons, make sure to first activate the Notify me toggle button on the Settings page.
  9. Once all conditions are set, on the top-right screen, tap Save (K).
    You can see the newly created action on the Quick tab. Tap on the action to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?