0100DB2301

Electric Power Fundamentals

Abstract: The fundamentals of electric power and electrical systems have remained unchanged for many years though technologies employed in electrical power systems have advanced greatly. Anyone responsible for any part of an electrical system relies on the fundamental relationships presented.

Introduction

The fundamentals of electric power and electrical systems have remained unchanged for many years, though technologies employed in electrical power systems have advanced greatly. Anyone responsible for any part of an electrical system relies on the fundamental relationships presented. An understanding of the fundamentals of electric power is vital to successful power system design. It is assumed that the reader has a degree in electrical power engineering or electrical power engineering technology, however the following discussion is presented as a review and reference material for completeness.

Basic Concepts

Commercial electric power in the United States is generated and delivered as alternating current, abbreviated as “AC”. AC power consists of sinusoidal voltages and currents. Mathematically, an AC voltage or current can be expressed as follows:

v(t) = Vmaxcos(360f·t+Фv)

(2–1)

i(t) = Imaxcos(360f·t+ФI)

(2–2)

Where:

  • v(t) is an AC voltage

  • i(t) is an AC current

  • Vmax is the voltage amplitude

  • Imax is the current amplitude

  • f is the system frequency

  • Фv is the voltage phase shift in degrees

  • Фt is the current phase shift in degrees

  • t is the time in ms

All angles are measured in degrees.

AC currents and voltages are economical to generate and, further, the magnitudes of the currents or voltages can be stepped up or down using transformers.

Three-phase AC power is the standard in the United States due to its convenience of generation. Three-phase (abbreviated “3Ф “) power is characterized by three different phases, each with a phase shift 120° from the other two phases. The three phases are typically referred to as “A”, “B”, and “C”. Further, the standard frequency for the United States is 60 Hz. Therefore, three-phase voltages in the United States can be mathematically described as follows:

va(t) = Vmaxcos(360x60xt) = Vmaxcos(21600t)

(2–3)

vb(t) = Vmaxcos(360x60xt – 120°) = Vmaxcos(21600t – 120°)

(2–4)

vc(t) = Vmaxcos(360x60xt +120°) = Vmaxcos(21600t + 120°)

(2–5)

Where:

  • va(t) is the A-phase voltage

  • vb(t) is the B-phase voltage

  • vc(t) is the C-phase voltage

The voltages from (2-3) – (2-5) are shown graphically in Graphical Representation of 3Ф Voltages.

Graphical Representation of 3Ф Voltages

The peaks of the voltage waveforms are 120° (5.5 ms at 60 Hz) apart. The peak of phase A occurs before the peak of phase B, which in turn occurs before the peak of phase C. This is referred to as an ABC phase sequence or ABC phase rotation. If any two-phase labels are swapped, the result is a CBA phase rotation. Both are encountered in practice. Also, the definition of time = 0 is arbitrary due to the periodic nature of the waveforms.

Because the full mathematical representation of AC voltages and currents is not practical, a shorthand notation is usually used. This shorthand notation treats the sinusoids as complex quantities based upon the following mathematical relationship:

cos(ө) = Re{e}

(2–6)

Where:

  • Re is the real part of the complex quantities

The voltage quantities from (2-3) – (2-5) can therefore be rewritten as follows:

va(t) = Re{Vmaxej21600t }

(2–7)

vb(t) = Re{Vmaxej(21600t –120°)}

(2–8)

vc(t) = Re{Vmaxej(21600t + 120°)}

(2–9)

To further develop this shorthand notation, it must be recognized that the use of the RMS (root-mean-square) quantity, rather than the amplitude, is advantageous in power calculations (discussed below). The RMS quantity for a periodic function f(t) is defined as follows:

(2–10)

Where:

  • Frms is the RMS value of the periodic function f(t)

  • T is the period of f(t)

Using (2-10), the RMS value of each of the sinusoidal voltages from (2-3) – (2-5) are calculated as:

Vrms = Vmax/√2

(2–11)

Because the RMS value is so useful in the calculation of power-related quantities, any time an AC voltage or current value is given it is assumed to be an RMS value unless otherwise stated.

Assuming only the real part of e is kept, the voltages from (2-7) – (2-9) can be written as complex quantities known as phasors:

a = Vmaxej21600t

(2–12)

b = Vmaxej(21600t –120°)

(2–13)

c = Vmaxej(21600t + 120°)

(2–14)

Assuming a frequency of 60 Hz, the commonly-used shorthand notation for (2-12) – (2-14) is:

a = Vmax∠0°

(2–15)

b = Vmax∠–120°

(2–16)

c = Vmax∠120°

(2–17)

The phasor quantities in (2-15) – (2-17) can be treated as complex quantities for the purposes of manipulation and calculation, but with the understanding that, if required, the basic time-domain voltage relationships of (2-3) – (2-5) can easily be obtained. The phasors can be plotted, as shown in Plot for Phasors per (2-15) – (2-17).

Plot for Phasors per (2-15) – (2-17)

In most instances the Re and Im axes are omitted since the definition of time zero (and thus angle zero) is arbitrary; the important information conveyed is the angular relationships between the phasors themselves. The real part of a phasor is its projection on the Re axis; if the phasors are imagined to rotate in a counter-clockwise direction about the 0,0 point it can be seen that the peak of va(t), represented by the tip of phasor V̄a crossing the Re axis, occurs first, followed by the peak of vb(t), followed in turn by the peak of vc(t). Thus, for angles defined as positive in the counter-clockwise direction the ABC phase sequence is indicated by a counter-clockwise phasor rotation. If angles are defined as positive in the clockwise direction a clockwise phasor rotation indicates an ABC phase sequence. Both are encountered in practice. In this guide all angles in phasor diagrams are assumed to be positive in the counterclockwise direction.

A very general representation of a 3Ф system is shown in General 3Ф System Representation.

General 3Ф System Representation

In Figure 4 the three phases A, B, and C have been labeled, along with the neutral (N) and ground (G). The neutral is optional, however the ground always exists. The AC voltages V̄a1, V̄b1, and V̄c1 per the discussion above could represent phase-to-phase voltages (V̄ab1, V̄bc1, V̄ca1), phase-to-neutral voltage. (V̄an1, V̄bn1, V̄cn1), or phase-to-ground voltages (V̄ag1, V̄bg1, V̄cg1). The existence of the neutral, and the relationship between the phases and ground, is dependent upon the system grounding and is discussed in System Grounding. A ground current is not defined; this is because the ground is not intended to carry load current, only ground fault current as discussed in subsequent sections of this guide. In practice, when 3Ф voltages are discussed, they are assumed to be phase-to-phase voltages unless otherwise noted.

AC Power

With the basic concepts per above, AC electrical power can be described.

Consider the following DC circuit element:

DC Circuit Element for Power Calculation

For the circuit element of DC Circuit Element for Power Calculation the following is true:

P= Vdc·Idc

(2–18)

Where:

  • Vdc is the DC voltage across the circuit element under consideration, with polarity as shown.

  • Idc is the DC current through the circuit element under consideration, considered positive for the direction shown.

  • P is the power generated by, or dissipated through, the circuit element under consideration.

The sign of P in (2-18) depends on the direction of current flow with respect to the DC voltage. A positive value for P indicates power dissipated, while a negative value for P indicates power generated. DC power is measured in Watts, where one Watt is 1 V x 1 A.

With AC voltages and currents the expression for power is more complex. Assume that one phase is taken under consideration, with an AC current and voltage as defined by (1-1) and (1-2) respectively. The expression for the instantaneous power, after some manipulation, is:

p(t) = v(t) i(t) = VmaxImax/2[cos(Фv - Фi) + cos(2πft + Фv + Фi)]

(2–19)

Thus, the instantaneous power consists of two parts: A DC component and an AC component with a frequency twice that of the system frequency. The quantity (Ф v - ФI) is defined as the power angle or power factor angle and is the angle by which the current peak lags behind the voltage peak on their respective waveforms. The quantity P= cos(Фv- ФI) is known as the power factor of the circuit.

The average value of p(t) is of concern in AC circuits. The average value of p(t) is:

P = VmaxImax/2 cos(Фv - Фi)

(2–20)

Recall that Vmaxcan be expressed in terms of Vrms per (2-11); substituting Vrmsper (2-11) into (2-20) yields:

P = VrmsIrmscos(Фv - Фi)

(2–21)

However, the absolute value of the product VrmsIrms cos(Фv - ФI) is always less than VrmsIrms unless (ᶲv - ФI) = 0. Further, if (ᶲv - ᶲI) = ±90º, as is the case with a purely inductive or capacitive load. VrmsIrms cos(ᶲv - ФI) = 0. Because energy is required to force current to flow, and energy is always conserved, AC power must have another component. This component is most easily defined if AC power is treated as a complex quantity. To do this, Complex Power S̄ is defined as follows:

S̄ = V̄ ·Ī*

(2–22)

The quantities V̄ and Ī are the AC current and voltage in their complex forms per (2-15) above, with the * operator denoting the complex conjugate, or angle negation, of the current. This conjugation of the current is done to yield the correct value for the power angle as described below. Real Power P and Reactive Power Q are defined as follows:

S̄ = P + jQ

(2–23)

P = Re{S̄} = VrmsIrmscos(Фv - Фi)

(2–24)

Q = Im{S̄} = VrmsIrmssin(Фv - Фi)

(2–25)

S = |S̄| = √P2+Q2

(2–26)

P is expressed in Watts. Q has the same units but to differentiate it from P it is expressed in Vars. rather than Watts. S is the Apparent Power and is also expressed in Volt-amperes.

The relationship between P, Q, S, S̄, and (Фv - ФI). can be shown graphically:

Graphical Depiction of AC Power

The depiction in Graphical Depiction of AC Power is referred to as the power triangle since P, Q, and S̄ form a right triangle. It is also important to note that the power factor angle is the same as the load impedance angle of the circuit. The power factor is referred to as a lagging power factor if the current lags the voltage (that is, (Фv - ФI) is positive up to 90º ) and as a leading power factor if the current leads the voltage (that is, (Фv - ФI) is negative down to -90º). For a lagging power factor, the real and reactive power flow is in the same direction; for a lagging power factor they flow in opposite directions. Of the passive circuit elements, resistors exhibit a unity power factor, inductors exhibit a 0 power factor lagging, and capacitors exhibit a 0 power factor leading.

The foregoing discussion considers only single-phase circuits. For 3Ф circuits the power quantities for all three phases must be added together, that is,

= S̄A + S̄B+ S̄C

(2–27)

P = PA + P B+ PC

(2–28)

Q = QA + QB+ QC

(2–29)

(2–30)

If the voltage magnitudes and power factor angles for each phase are equal, the power quantities per phase can be represented as S̄, S , P, Q; equations (2-27) – (2-30) can then be simplified as:

= 3S̄

(2–31)

= 3P̄̄

(2–32)

Q = 3Q

(2–33)

S = 3S

(2–34)

Transformers

Transformers are vital components for AC power systems. They are used to change the voltage and current magnitudes to suit the application.

The Ideal Transformer

Transformers are relatively simple devices that utilize Faraday’s law of electromagnetic induction. In its simplest form, this law can be written:

ξ = -N dψ/dt

(2–35)

Where ξ is the voltage induced in a coil of N turns that is linked by a magnetic flux Ψ.

In turn, the magnetic flux Ψ for a coil of N turns through which a current I passes and linked by a magnetic path with reluctance ℜ can be expressed as:

Ψ = NI/ℜ

(2–36)

Consider the simple transformer shown in Basic Transformer Model:

Basic Transformer Model

From (2-35) and (2-36):

Ψ=(N1 I1)/ℜ = (N2 I2)/ℜ

(2–37)

⇒ N1 I1 = N2 I2

(2–38)

⇒ I1 = N2/NI1I2

(2–39)

V1 = -N1dΨ/dt = -(N12/ℜ)dI1/dt = -(N1N2/ℜ)dI2/dt

(2–40)

V2 = -N2dΨ/dt = -(N22/ℜ)dI2/dt

(2–41)

Dividing (2-40) by (2-41),

V1/V2 = N1/N2

(2–42)

Equations (2-38) and (2-42) are the basic equations for a single-phase transformer. The voltage ratio (V1/V2) is equal to the turns ratio (N1/ N2), and the current ratio is equal to the inverse of the turns ratio. By re-writing (2-38) in terms of the turns ratio (N1/N2) and substituting into (2-42), the following is obtained:

V1I1 = V2/I2

(2–43)

This is to be expected, since the apparent flowing into the transformer should ideally equal the apparent power flowing out of the transformer.

The usefulness of the transformer lies in the fact that it can adjust the voltage and current to the application. For example, on a transmission line it is advantageous to keep the voltage high to be able to transmit the power with as small a current as possible, to minimize line losses and voltage drop. At utilization equipment, it is advantageous to work with low voltages that are more conducive to equipment design and personnel safety.

Another important aspect of the transformer is that it changes the impedance of the circuit. For example, if an impedance Z̄2 is connected to winding 2 of the ideal transformer in Practical Transformer Model it can be stated that:

2 = I1 = V̄2/I2

(2–44)

Using (2-38) and (2-42), (2-44) can be written in terms V̄1 and Ī1:

2 = (N2/N1)V̄1/(N1/N2)/Ī1 = (N2/N1)2(V̄11

(2–45)

By definition:

1 = V̄1/(N1

(2–46)

Therefore, (2-45) can be re-written as:

2 = (N2/(N1)21

(2–47)

The impedance through the transformer is the load impedance at the transformer output winding multiplied by the square of the turns ratio.

A Practical Transformer Model

The idealized transformer model just presented is not sufficient for practical electric power applications since the core is not lossless and not all the magnetic flux links both sets of windings. To take this into account, a more realistic model is used:

Practical Transformer Model

The resistance Rc represents the core losses due to hysteresis, and inductance Lc represents the magnetizing inductance. Resistances R1 and R2 represent the winding resistances of winding 1 and winding 2, respectively. Inductances L1 and L2 represent the leakage inductances of windings 1 and 2, respectively. For quick calculations, the core losses and magnetizing inductance are often ignored, and the model is treated as an impedance in series with an ideal transformer.

To denote the proper polarity, the circuit representation for a transformer includes polarity marks as shown in Standard Transformer Symbolic Representation. If the current for one winding flows into its terminal with the polarity mark, the current for the other winding flow out of its terminal with the polarity mark. In addition, the ANSI polarity markings per IEEE Standard Terminal Markings and Connections for Distribution and Power Transformers* are shown; “H” denotes the higher voltage winding, and “X” denotes the lower voltage winding.

Standard Transformer Symbolic Representation

3Ф Transformer Connections

To be useful in 3Ф systems transformers must be connected for use with 3Ф voltage. This is accomplished using 3Ф transformer connections.

The wye-wye connection is shown in Wye-Wye Transformer Connection. This could be a bank of three single-phase transformers or one 3Ф transformer which consists of all three sets of windings on a common ferromagnetic core. Polarity markings for three single-phase transformer connections are shown at the individual transformers, and polarity markings for a 3Ф transformer are shown next to the A, B, C, and N terminals.

For both the primary and secondary windings the magnitude of the line-to-line voltage is equal to the magnitude of the line-to-neutral voltage multiplied by √3. For convenience, the transformer turns ratio is taken as 1:1 on the phasor diagram.

Wye-Wye Transformer Connection

If a three-phase transformer is used, the wye-wye connection has the disadvantage of requiring a four-legged core to allow for a magnetic flux imbalance. Further, the solidly-grounded neutrals allow for ground currents to flow that can create interference in communications circuits (see Electric Power Distribution System Design, New York* Both the primary and secondary neutrals terminals must be solidly grounded to allow for triple-harmonic currents to flow; if the neutrals are allowed to float, harmonic overvoltages are developed from phase to neutral on each winding. These overvoltages can damage the transformer insulation. Wye-wye transformers are often used on systems above 25 kV to minimize a problem known as ferroresonance. Ferroresonance is a condition which results from the transformer magnetizing impedance resonating with the upstream cable charging capacitance, resulting in destructive overvoltages as the transformer core moves into and out of saturation in a non-linear manner. Single-phase switching is usually the cause of ferroresonance.

The delta-delta connection is shown in Delta-Delta Transformer Connection. There is no neutral on the delta-delta connection. A unique feature of this connection is that if one transformer is taken out of service, the two remaining transformers still provide three-phase service at a reduced capacity (57.7% of the capacity with all three transformers in service).

Delta-Delta Transformer Connection

The delta-wye connection is shown in Delta-Wye Transformer Connection. Note that for the given turns ratios of 1:1 that the magnitude of the phase-to-phase output voltage is equal to the magnitude of the phase-to-phase input voltage multiplied by √3. The input and output voltages of 3Ф transformers and 3Ф banks of single-phase transformers are always referenced as the phase-to-phase magnitude. Therefore, for a delta-wye transformer the winding turns ratios for each set of windings must be compensated by (1/√3) to produce the desired input-to-output voltage ratio. The phase-to-phase voltages on the lower voltage side of the transformer lag the phase-to-phase voltages on the high voltage side by 30°. This is dictated by IEEE Standard Terminal Markings and Connections for Distribution and Power Transformers*.

The delta-wye transformer connection is by far the most popular choice for commercial and industrial applications. 3Ф transformers do not require a four-legged core like the wye-wye connection, but the advantages of a wye secondary winding (elaborated on in System Grounding) are obtained. Further, the secondary neutral can be left unconnected in this arrangement, unlike the wye-wye arrangement.

Delta-Wye Transformer Connection

The wye-delta connection is shown in Wye-Delta Transformer Connection. This connection is seldom used in commercial and industrial applications. The delta is arranged differently from the delta-wye connection, to satisfy the requirement from IEEE Standard Terminal Markings and Connections for Distribution and Power Transformers* to have the phase-to-phase voltages on the low-voltage side of the transformer lag the corresponding voltages on the primary side by 30°.

Wye-Delta Transformer Connection

Parallel Operation of Transformers

For supplying a load in excess of the rating of an existing transformer, two or more transformers may be connected in parallel with the existing transformer. The transformers are connected in parallel when the load on one of the transformers is more than its capacity. The reliability is increased with parallel operation than to have single larger unit. The cost associated with maintaining the spares is less when two transformers are connected in parallel. The most essential condition for successful parallel operation of transformers are:

  • The voltage rating of both primaries and secondaries should be identical, for example, the transformers should have the same turn ratio.

  • The percentage impedances should be equal in magnitude and have the same X/R ratio to avoid circulating currents and operation in different power factor.

  • The polarity of the two transformers should be the same.

  • Phase sequences and phase angle shifts must be the same (for three-phase transformer).

Transformer Vector Group

The vector group is used to identify the phase shift between the primary and secondary windings. In the vector group, the secondary voltage may have the phase shift of 30° lagging or leading, 0° for example, no phase shift or 180° reversal with respect to the primary voltage.

The transformer vector group is labeled by capital and small letters plus numbers from 1 to 12 in a typical clock-like manner; the capital letter indicates primary winding and small letter represents secondary winding as shown in Transformer Vector Group Label:

Transformer Vector Group Label

Basic Electrical Formulae

The following formulae are given as a convenient reference for the reader. These formulae include both formulae derived in this section and those basic formulae which are derived from basic circuit theory.

DC Circuits

Vdc = IdcRdc

(2–48)

P = Vdc = IdcIdc

(2–49)

P = Idc2Rdc = Vdc2/Rdc

(2–50)

Where:

  • Vdc is the DC voltage across the circuit element under consideration.

  • Idcis the current through the circuit element under consideration. Idcis considered positive if it flows from the circuit element terminal at the higher voltage to the terminal at the lower voltage.

  • Rdcis the DC resistance of the circuit element under consideration, measured in Ohms.

  • P is the power dissipated or generated by the circuit element.

P is the power dissipated or generated by the circuit element. A positive power from (2-49) indicates power dissipated by the circuit element, and a negative value indicates power generated by the circuit element. The sign of P in (2-50) is lost due to the squaring of the current or voltage.

Passive Energy Storage Elements

Capacitors store energy in the form of voltage, with governing equations:

ic = Cdvc/dt

(2–51)

E = i/2Cvc2

(2–52)

Where:

  • vc is the voltage across the capacitor.

  • Ic is the current through the capacitor, considered positive if it flows toward the terminal from which vc is referenced.

  • C is the capacitance value of the capacitor, measured in Farads.

  • E is the energy stored in the capacitor.

Inductors store energy in the form of current, with governing equations:

vi = LdiI/dt

(2–53)

E = 1/2Li2

(2–54)

Where:

  • vI is the voltage across the inductor.

  • II is the current through the inductor, considered positive if it flows toward the terminal from which vI is referenced.

  • L is the inductance value of the inductor, measured in Henries.

  • E is the energy stored in the inductor.

AC Voltages and Currents, Time-domain Form

Single-phase AC voltage and current can be expressed as follows:

v(t) = Vmaxcos(360ft + Фv

(2–55)

i(t) = Imaxcos(360ft + ФI

(2–56)

Where:

  • vtis an AC voltage.

  • II is an AC current.

  • Vmax is the voltage amplitude.

  • Imax is the current amplitude.

  • f is the system frequency.

  • Фvis the voltage phase shift in degrees.

  • Фi is the current phase shift in degrees.

  • t is the time in milliseconds.

All angles are measured in degrees.

If the frequency is 60 Hz, 3Ф voltages can be written as:

va(t) = Vmaxcos(360x60xt) = Vmaxcos(21600t)

(2–57)

vb(t) = Vmaxcos(360x60xt – 120°) = Vmaxcos(21600t – 120°)

(2–58)

vc(t) = Vmaxcos(360x60xt +120°) = Vmaxcos(21600t + 120°)

(2–59)

Where:

  • Va(t) is the A-phase voltage.

  • Vb(t) is the B-phase voltage.

  • Vc(t) is the C-phase voltage.

The RMS value of a perfectly sinusoidal AC voltage or current is:

Vrms = Vmax/√2

(2–60)

Irms = Imax/√2

(2–61)

AC Power, Time-domain Form

The instantaneous single-phase AC power resulting from a current per (2-56) flowing through a circuit element with voltage (2-55) across it is:

p(t) = v(t)i(t) = VmaxImax/2[cos(Фv - Фi) + co(2πft + Фv + ФI)]

(2–62)

Where all terms are as defined for (2-54) and (2-55).

The average power in this case is:

P = VmaxImax/2 cos(Фv - Фi)

(2–63)

P = VrmsIrmscos(Фv - Фi)

(2–64)

Where P is the average power.

AC Currents, Voltages and Circuit Elements, Frequency-domain Form

Assuming only the real part is kept when converting to time-domain and that the same frequency applies throughout, AC currents and voltages can be written in the frequency domain as:

V̄ = VrmsФv

(2–65)

Ī̄ = ĪrmsФI

(2–66)

Where:

  • V̄ is the AC voltage in frequency-domain form.

  • Ī is the AC current in frequency-domain form

  • Фv is the voltage phase shift.

  • ФI is the current phase shift.

Capacitor and Inductor impedances in frequency domain form are:

c = 1/j2πfC

(2–67)

I= j2πfL

(2–68)

Where:

  • cis the impedance of the capacitor.

  • lis the impedance of the inductor.

  • j = √(-1).

  • f is the system frequency.

  • C is the capacitance of the capacitor .

  • L is the inductance of the inductor.

AC voltage and current for an impedance Z̄ are related as follows:

V̄ = Ī·

(2–69)

Average single-phase power in AC form can be expressed as:

S̄ = V̄· Ī*̄

(2–70)

Where S̄ is the complex power.

Complex power S̄ can be separated into real power P and reactive power Q:

S̄ = P + jQ

(2–71)

P = Re{S̄} = VrmsIrmscos(Фv - Фi)

(2–72)

Q = Im{S̄} = VrmsIrmssin(Фv - Фi)

(2–73)

S = |S̄| = √(P2 + Q2 )

(2–74)

For 3Ф circuits the total power is the sum of the power in each phase, that is,

3Ф = S̄A + S̄B + S̄C

(2–75)

P3Ф = PA + PB + PC

(2–76)

Q3Ф = QA + QB + QC

(2–77)

(2–78)

If the current and voltage magnitudes and angles are equal for each phase, (2-76) – (2-78) can be simplified as follows by considering the power quantities per phase to be S̄ ,S, P, and Q:

3Ф = 3S̄1Ф

(2–79)

P3Ф = 3P1Ф

(2–80)

Q3Ф = 3Q1Ф

(2–81)

S3Ф = 3S1Ф

(2–82)

Basic Transformers

The input voltage and current V1 and I1 and the output voltage and current V2 and I2 for an ideal single-phase transformer are related as follows:

N1I1 = N2I2

(2–83)

V1/V2 = N1/N2

(2–84)

The impedance Z̄1at the input terminals of a transformer is related to the load impedance Z̄2connected to the transformer output terminals by the following equation:

1 = (N1/N2)22

(2–85)

References

Because the subject matter for this section is basic and general to the subject of electrical engineering, it is included in most undergraduate textbooks on basic circuit analysis and electric machines. Where material is considered so basic as to be axiomatic no attempt has been made to cite a particular source for it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.