0100DB2301

Electrical Vehicle Charging

Abstract: Electric vehicle (EV) adoption has rapidly increased in the past decade and is projected to continue growing exponentially. With it comes the need for a new fueling paradigm that adds heavy loading to the electrical system. EV drivers interact with different types of chargers based on the application. System designers need to consider how the user will interact with the charger, what charging behavior should be encouraged, the overall size of the system, effective power distribution equipment, and charge management software with monitoring and control capabilities to specify the optimal EV charging site.

Introduction

Electric Vehicle Supply Equipment (EVSE, commonly referred to as electric vehicle chargers or EV chargers) is becoming a more common electrical load as EV demand rises. Most top automakers who sell to the US market have made commitments to dramatically increase production of electric vehicles within the next two decades. Designing systems with EVSE as a load requires several special considerations. This section will examine NEC requirements for electric vehicle supply equipment installations, types of electric vehicle chargers, an overview of standards to consider when specifying a charger or designing a system to support it, power distribution equipment to support EVSE installations, smart charging and charge management systems, and the emerging application of bidirectional charging.

NEC 625 Electric Vehicle Power Transfer System

NEC National Electric Code® Article 625 covers the electrical conductors and equipment connecting an electric vehicle to premises wiring for the purposes of charging, power export, or bidirectional power flow. To understand these requirements, the basic NEC definitions of Electric Vehicle Supply Equipment and related terms as provided in Article 100 must be understood.

NOTE: This guide is not intended as a substitute for familiarity with the NEC, nor is it intended as an authoritative interpretation of every aspect of the NEC articles mentioned.

Electric Vehicle: An automotive-type vehicle for on-road use, such as passenger automobiles, buses, trucks, vans, neighborhood electric vehicles, and electric motorcycles, primarily powered by an electric motor that draws current from a rechargeable storage battery, fuel cell, photovoltaic array, or other source of electric current. Plug-in hybrid electric vehicles (PHEV) are electric vehicles having a second source of native power.

Electric Vehicle Connector: A device that, when electrically coupled (conductive or inductive) to an electric vehicle inlet, establishes an electrical connection to the electric vehicle for power transfer and information exchange.

Electric Vehicle Power Export Equipment (EVPE): The equipment, including the outlet on the vehicle, that is used to provide electrical power at voltages greater than or equal to 30 Vac or 60 Vdc to loads external to the vehicle, using the vehicle as the source of supply.

Electric Vehicle Supply Equipment (EVSE): Equipment for plug-in charging, including the ungrounded, grounded, and equipment grounding conductors, and the electric vehicle connectors, attachment plugs, personnel protection system, and all other fittings, devices, power outlets, or apparatus installed specifically for the purpose of transferring energy between the premises wiring and the electric vehicle.

Wireless Power Transfer Equipment (WTPE): Equipment installed specifically for transferring energy between the premises wiring and the electric vehicle without physical electrical contact.

NOTE: The general form of WTPE consists of two physical packages: a control box and a primary pad.
NOTE: Electric vehicle power export equipment and wireless power transfer equipment are sometimes contained in one set of equipment, sometimes referred to as a bidirectional WPTE.

DCFC: DC Fast Charger, also referred to as Level 3.

Battery Management System (BMS)

  • Regulates the current and voltage supplied to the battery and optimizes the charging process.

  • Communicates with the vehicle’s onboard computer in-regards to the charging process.

  • Monitors the charging process.

Electromagnetic Interference (EMI): EMI can disrupt the normal functioning of electronic systems in an EV, such as the audio, GPS, engine control unit, and more. It can also interfere with other electronic equipment nearby. Filters and shielding can be employed.

BESS: Battery Energy Storage System - Captures energy from renewable and non-renewable sources and stores it in rechargeable batteries for later use.

DER: Distributed Energy Resources - A distributed energy resource is any resource or technology that generates, stores, or manages energy at a local level, typically close to the point of consumption.

With these definitions in mind, NEC 625 includes standards for design considerations for power distribution equipment and energy management software, both of which will be discussed in greater detail later in this design guide. A selection of relevant sections is included in the following.

625.40 Electric Vehicle Branch Circuit. Each outlet installed for the purpose of supplying EVSE greater than 16 amperes or 120 volts shall be supplied by an individual branch circuit. Exception: Branch circuits shall be permitted to feed multiple EVSEs as permitted by 625.42(A) or (B).

625.41 Overcurrent Protection. Overcurrent protection for feeders and branch circuits supplying EVSE and WTPE, including bidirectional EVSE and WPTE, shall be sized for continuous duty and shall have a current rating of not less than 125 percent of the maximum load of the equipment. Where noncontinuous loads are supplied from the same feeder, the overcurrent device shall have a current rating of not less than the sum of the noncontinuous loads plus 125 percent of the continuous loads.

625.42 Rating. The EVSE shall have sufficient rating to supply the load served. Electric vehicle charging loads shall be considered to be continuous loads for the purposes of this article. Service and feeder shall be sized in accordance with the product ratings, unless the overall rating of the installation can be limited through controls as permitted by 625.42(A) or (B).

  1. Energy Management System (EMS). Where an EMS in accordance with 750.30 provides load management of EVSE, the maximum equipment load on a service and feeder shall be the maximum load permitted by the EMS. The EMS shall be permitted to be integral to one piece of equipment or integral to a listed system consisting of more than one piece of equipment. When one or more pieces of equipment are provided with an integral load management control, the system shall be marked to indicate this control is provided.

  2. EVSE with Adjustable Settings. EVSE with restricted access to an ampere adjusting means complying with 750.30(C) shall be permitted. If adjustments have an impact on the rating label, those changes shall be in accordance with manufacturer’s instructions, and the adjusted rating shall appear on the rating label with sufficient durability to withstand the environment involved. EVSE as references shall be permitted to have ampere ratings that are equal to the adjusted current setting.

625.43 Disconnecting Means. For EVSE and WPTE rated more than 60 amperes or more than 150 volts to ground, the disconnecting means shall be provided and installed in a readily accessible location. If the disconnecting means is installed remote from the equipment, a plaque shall be installed on the equipment denoting the location of the disconnecting means. The disconnecting means shall be lockable open in accordance with 110.25.

625.48 Interactive Equipment. EVSE or WTPE that incorporates a power export function and that is part of an interactive system that serves as an optional standby system, an electric power production source, or a bidirectional power feed shall be listed and marked as suitable for that purpose. When used as an optional standby system, the requirements of Parts I and II of Article 702 shall apply; when used as an electric power production source, the requirements of Parts I and II of Article 705 shall apply. EVPE that provides a receptacle outlet as its point of power export shall be in accordance with 625.60.

625.49 Island Mode. EVPE and bidirectional EVSE that incorporate a power export function shall be permitted to be a part of an interconnected power system operating in island mode.

625.50 Location. The EVSE shall be located for direct electrical coupling of the EV connector (conductive or inductive) to the electric vehicle. Unless specifically listed and marked for the location, the coupling means of the EVSE shall be stored or located at a height of not less than 450 mm (18 in.) above the floor level for indoor locations or 600 mm (24 in.) above the grade level for outdoor locations. This requirement does not apply to portable EVSE constructed in accordance with 625.44(A).

625.54 Ground-Fault Circuit-Interrupter Protection for Personnel. All receptacles installed for the connection of electric vehicle charging shall have ground-fault circuit-interrupter protection for personnel.

Types of Electric Vehicle Chargers

Electric vehicles (EVs) use batteries as a power source for locomotion. The battery in the EV is a direct current (DC) device and must be recharged with DC power. However, most power distribution systems run on AC power. To get power from a traditional site’s electrical system to the EV battery, it must be rectified from AC to DC before reaching the battery. This can be accomplished in one of two ways: the power conversion can happen inside the vehicle using its onboard charger (AC charging) or externally to the vehicle (DC charging). The following diagrams illustrate how EV batteries can be charged.

DC Charging Power Flow

AC Charging Power Flow

The charging speed of an electric vehicle is determined by the limiting factor (lower kW rating) of the onboard and offboard charging systems.

Charging Type Maximum charge rate is the lesser rating of these
AC Charging On-board Rectifier AC EVSE
DC Charging Max. Battery Acceptance Rate DC EVSE

The true instantaneous charging rate will vary depending on the battery’s charging curve, state of charge, internal and ambient temperature, and other factors. However, an approximation of total time to charge may be calculated thusly:

Time to charge = Battery Rating (kWh)  
EVSE Rating (kW)  

Two main considerations for EV charger selection will be discussed in this section. First, the power level of the EVSE, which determines how long it will take to recharge the EV battery. Second, the connector type, which is the interface for power and communications between the EVSE and the vehicle.

There are three widely used rates of EV charging: Level 1 AC, Level 2 AC, and Level 3 DCFC. Electric vehicles can be used with different EVSE depending on the rate of charge / charging dwell-time desired.

Level 1 provides charging through a standard 120 V outlet. It is common in residential applications. AC power travels to the vehicle’s on-board charger, which rectifies it to DC power to charge the EV battery. Level 1 charging adds two to five miles to the battery range per hour of charge, taking 40–50 hours to completely fill a vehicle battery.

Level 2 charging follows the same path as Level 1 charging (AC power -> onboard charger -> vehicle battery) through electric vehicle supply equipment (EVSE) rather than a standard 120 V outlet. The EVSE may be applied at 208/120 V or 240 Vac. The upstream overcurrent protective device for a Level 2 EVSE will be a two-pole breaker rated at least 125% of the rated EVSE current (e.g., a Level 2 EVSE rated for 30 A would be fed from a 40 A 2P breaker). Level 2 EVSE is commonly seen in residential, workplace, and public charging applications. They can fill an all-electric battery in 4–10 hours.

Common Level 2 ratings and their upstream overcurrent protective device ratings:

AC Level 2 EVSE Charger Output Upstream OCPD
7.2 kW 30 A 40 A 2P
7.6 kW 32 A 40 A 2P
9.6 kW 40 A 50 A 2P
11.5 kW 48 A 60 A 2P
16.8 kW 70 A 90 A 2P
19.2 kW 80 A 100 A 2P

The following table approximates different dwell times and corresponding range added to an EV plugged into an AC Level 2 charger.

Site Application Residential Workplace Shopping Mall Stores
Charge Time 8–12 hours 8 hours 1–2 hours 30–60 minutes
Extra Range 30–200 miles 30–100 miles 10–60 miles 10–40 miles

Average charging time of a typical electric passenger vehicle for a 25-mile trip:

DCFC Level 3 Direct Current Fast Charge (DCFC) equipment is the fastest way to charge an EV battery due to its higher kW rating. DCFC EVSE power ratings range from 20 kW up to 350 kW. Instead of using the vehicle’s onboard charger to convert from AC to DC, the DCFC EVSE takes care of the power conversion and pushes DC power to an onboard DC/DC converter then directly to the vehicle battery.

DCFC is typically fed from 480 V 3P breakers. DC fast chargers are typically installed along highways for public use, or for fleet vehicles or car dealerships that need a quick charging turnaround. DCFC can get a battery from zero to 80% in as little as 20 minutes.

There are two commonly available configurations for DCFC: Standalone or “All In One” systems and Split systems.

Standalone (SA): or “All in One” systems normally < 240 kWpp (max around 480 kW). Modules combined with charger.

Split systems: Separated dispenser and power module cabinet. Normally 150 kW-360 kW max pp (max 500 kW) but similar architecture for MW. Shared power amongst multiple dispensers, normally (1–8 ports), some systems are scalable with additional modules or cabinets.

The following is a list of common DCFC ratings. Upstream overcurrent protection device sizes should be confirmed with the manufacturer’s datasheet.

DCFC EVSE Ratings:

  • 30 kW

  • 50 kW

  • 60 kW

  • 75 kW

  • 100 kW

  • 120 kW

  • 150 kW

  • 180 kW

  • 250 kW

  • 350 kW

Connectors

In addition to different rates of charging, connector type is a consideration when selecting an EV charger. In North America, the most common standards are SAE J1772 for AC charging and Combined Charging Standard 1 (CCS1) for DC charging, or the North American Charging Standard (NACS, formerly known as Tesla) for both AC and DC charging. Some vehicles, like older models of the Nissan Leaf, use a CHAdeMO connector, but these are being phased out.

Nearly one million EVs on the road at the beginning of 2024 use J1772 for AC charging and CCS1 for DC charging. However, now that NACS is available for vehicles other than Tesla, many automakers will be switching to the NACS connector and standard. Ford, GM, VW Group (including Audi and Porsche), BMW Group, Mercedes-Benz, Hyundai, Genesis, Kia, Mazda, Nissan/Infiniti, Toyota/Lexus, Subaru, Volvo, Polestar, Lucid, Fisker, and Rivian have all committed to using the NACS configuration in 2025.

Type 1–SAE J1772

This is the standard for Level 1 and 2 charging in North America and Asia, where the source is a single-phase alternating current (AC). It is a 5-pin plug that can draw power up to 19.2 kW.

Type 2–Mennekes

This is the standard in Europe where triple-phase alternating current is the default power source for Level 1 and 2 charging. The 7-pin plug allows up to 43 kW and (unlike the Type 1) features an automatic locking mechanism to prevent accidental disconnection.

CCS1

This 7-pin EV plug is used for DCFC charging (up to 350 kW) in North America, although it can also be used for slow AC charging. Essentially, the CCS1 is a SAE J1772 plug with two additional high-speed DC charging pins added.

CCS2

The European counterpart of the CCS1 is a 9-pin enhancement of the Mennekes plug. It allows charging of up to 350 kW. As with the CCS1, this plug can deliver both AC and DC charging.

CHAdeMO

Initially developed in Japan, the 10-pin CHAdeMO was one of the first fast-charging DC plug types on the market. The first generation offered up to 50 kW, and the second generation expanded to 400 kW. Despite its popularity in Japan, the plug is being phased out internationally, particularly since the European Commission mandated CCS2 for DC charging in Europe.

GB/T

GB/T is the standard AC and DC plug in China, delivering 7.4 kW for AC and 237.5 kW for DC. It is used by around half the electric vehicles in the world today but is not used in North America.

North American Charging Standard (NACS)

Tesla’s formerly proprietary EV plug accommodates Level 1, 2 and 3 AC and DC charging. In other words, there is just the one plug. In Europe, Tesla cars now use CCS2 charging.

EV Charging Connector Types

As manufacturers switch their plug standard and the industry evolves, adaptors and cable kits help drivers use a multitude of EV chargers. All Tesla vehicles come with an adapter that connects to the J1772 plug. An adaptor that goes the other way, allowing J1772/CCS1 vehicles to use NACS chargers, is also available. Many charging companies are also offering the option to retrofit their stations with a new cord to keep up with the industry’s increased adoption of NACS.

Electric Vehicle Charging Standards

Industry standards are changing rapidly as this growing industry evolves. There are published and developing standards regarding conductive and inductive charging, unidirectional charging and bidirectional power transfer, charger construction and safety, communication, cybersecurity, and more. The Electric Vehicle Charging Standards table below classifies various standards pertinent to electric vehicle charging systems but is not intended to be comprehensive. Many local, state, and regional jurisdictions may also be relevant.

Standard/Recommended Practical Guide

Title Description

NFPA 70 (NEC) Article 625

Electric Vehicle Charging System 

Covers the installation of equipment and devices external to an electric vehicle related to electric vehicle charging.

International Building Code (IBC)

2021 Electric Vehicles and Building Codes: A Strategy for Greenhouse Gas Reductions

Provides example code language for municipalities to set their own policies. Notably, it defines the minimum EV circuit size as 40 A and 208/240 V. Provides table for municipalities to define percentage of parking stalls as EVSE installed, EV-capable, and EV-ready for new construction.

IEEE C62.230-2022

IEEE Guide for Surge Protection of Electric Vehicle Infrastructure

Outlines the application of surge-protective devices for electric vehicle infrastructure including power, data acquisition, and communications-related circuitry.

IEEE 2030.5

IEEE Standard for Smart Energy Profile Application Protocol

Defines the application layer with TCP/IP providing functions in the transport and Internet layers to enable utility management of the end user energy environment, including demand response, load control, time of day pricing, management of distributed generation, and electric vehicles.

UL 2202

DC Charging Equipment for Electric Vehicles

Covers off board electric vehicle conductive charging equipment that converts from AC to DC (DC output devices) to recharge the propulsion batteries in over-the-road electric vehicles. Does not cover on board EV chargers.

UL 2594

Electric Vehicle Supply Equipment

Covers off board electric vehicle conductive charging equipment that does not convert voltage (AC in – AC out) and provides power to an onboard EV charger.

UL 2231

Standard for Personnel Protection Systems for Electric Vehicle (EV) Supply Circuits

Includes general requirements for EV supply circuits to reduce the risk of electric shock to the user from accessible parts in grounded or isolated circuits for charging electric vehicles. These circuits are external to or on board the vehicle. This standard also includes particular requirements for protection devices for use in charging systems, including requirements for isolated circuit capacitor switching transient testing and harmonic distortion immunity testing.

UL 2251

Standards for Safety: Plugs, Receptacles, and Couplers for Electric Vehicles

Standard for safety regarding EV plugs, EV receptacles, vehicle inlets, vehicle connectors, and EV breakaway couplings under conditions of continuous use. These devices are intended for use with conductive EVSE and are intended to facilitate the conductive connection from the EVSE to the vehicle.

UL 2252

Outline of Investigation for Adapters for use with Electric Vehicle Couplers

Investigates adapters for conductive EV power transfer to the vehicle. The adapters are not used to convert voltages. They are only used to convert the physical configuration of the interfaces and provide for continued communication protocols.

UL 2263

Electric Vehicle Cable

This standard specifies the requirements for electric vehicle cables rated up to 1000 Vac and DC intended to be part of a cord set carried in the vehicle for connection to a charging station or for permanent or temporary connection to Electric Vehicle Supply Equipment (EVSE) or for connection to the branch circuit supplying the EVSE or vice versa.

SAE J1772

SAE Standard for Electric Vehicle and Plug-in Hybrid Electric Vehicle Conductive Charge Coupler 

This SAE standard covers physical, electrical, functional, safety, and performance requirements for conductive power transfer to an electric vehicle, including operational requirements and the functional and dimensional requirements for the vehicle inlet and mating connector.

SAE J3400

North American Charging System (NACS) for Electric Vehicles

This standard is currently a work in progress. It will cover physical, electrical, functional, safety, and performance requirements for conductive power transfer to an electric vehicle using a connector capable of transferring either DC or AC single-phase power using two current-carrying contacts.

SAE J2344

Guidelines for Electric Vehicle Safety Equipment (EVSE)

This SAE Information Report identifies and defines the preferred technical guidelines relating to safety for vehicles that contain high voltage, such as Electric Vehicles (EV), Hybrid Electric Vehicles (HEV), Plug-In Hybrid Electric Vehicle (PHEV), and Fuel Cell Vehicles (FCV) during normal operation and charging. Guidelines in this document do not necessarily address maintenance, repair, or assembly safety issues

NECA 413-2019

Installing and Maintaining Electric Vehicle Supply Equipment (EVSE)

Procedures for installing and maintaining AC and DC EVSE.

Inductive Wireless EV Charging

UL 2750

Wireless Power Transfer Equipment for Electric Vehicles

Wireless Power Transfer (WPT) Equipment for transferring power to a stationary electric vehicle. WPT equipment consists of at least two devices, the power source, and a ground assembly. The WPT equipment may also be provided with a third device, the mating vehicle assembly. These requirements are also suitable for covering each individual device as a stand-alone product.

SAE J1773

SAE Recommended Practice for Electric Vehicle Inductively Coupled Charging

This SAE Recommended Practice establishes the minimum interface compatibility requirements for electric vehicle inductively coupled charging for North America that transfers power at frequencies significantly higher than power line frequencies. It is not applicable to inductive coupling schemes that employ automatic connection methods or that transfer power at power line frequencies.

Bidirectional EV Charging

UL 9741

Electric Vehicle Power Export Equipment (EVPE)

UL9741 covers off-board unidirectional and bidirectional equipment that transfers electrical energy between an electric vehicle and off board loads as well as operating in parallel with an electric power system, such as the electric utility grid, using a permanently attached vehicle connector. Equipment that has optional bidirectional functionality serves as both Electric Vehicle Power Export Equipment (EVPE) and electric vehicle supply equipment (EVSE). The power export functionality includes enable and disable functions to limit or prevent export to the utility grid for locations that are not capable of or permitted to receive back feed power. This functionality is addressed using requirements of UL 1741. The equipment performs power conversion and Interconnection Systems Equipment (ISE) functionality. These functions may be located within one piece of equipment or within multiple pieces of equipment.
Megawatt Charging

UL 2278

Outline of Investigation for Megawatt Charging Configured Electric Vehicle Couplers

These requirements cover vehicle connectors and vehicle inlets designated as, and configured as, megawatt charging couplers. These devices are rated up to 1500 Vdc, 1000 A under conditions of continuous use. Vehicle connectors may be actively cooled, such as with liquid cooling, when operating. These devices are intended for use with conductive DC charging equipment for electric vehicles and intended to facilitate conductive connection from the charging equipment to the vehicle.

SAE J3271

Megawatt Charging System for Electric Vehicles (Work In Progress)

This document describes the megawatt-level DC charging system requirements for couplers/inlets, cables, cooling, communication, and interoperability. The intended application is for commercial vehicles with larger battery packs requiring higher charging rates for moderate dwell time. Improving charging session reliability while maintaining existing number of contacts/conductors can be achieved by superimposing communication signals over “connection-detection” analog signals.

Historical / Stabilized Standards

SAE J2293/1

SAE Recommended Practice for Energy Transfer System for Electric Vehicles Part 1: Functional Requirements and System Architectures

SAE J2293 establishes requirements for Electric Vehicles (EV) and the off-board Electric Vehicle Supply Equipment (EVSE) used to transfer electrical energy to an EV from an Electric Utility Power System (Utility) in North America. This document defines, either directly or by reference, all characteristics of the total EV Energy Transfer System (EV-ETS) necessary to insure the functional interoperability of an EV and EVSE of the same physical system architecture. The ETS, regardless of architecture, is responsible for the conversion of AC electrical energy into DC electrical energy that can be used to charge the Storage Battery of an EV, as shown in Figure 1.

The different physical ETS system architectures are identified by the form of the energy that is transferred between the EV and the EVSE, as shown in Figure 2. It is possible for an EV and EVSE to support more than one architecture.

This document does not contain all requirements related to EV energy transfer, as there are many aspects of an EV and EVSE that do not affect their interoperability. Specifically, this document does not deal with the characteristics of the interface between the EVSE and the Utility, except to acknowledge the Utility as the source of energy to be transferred to the EV.

The functional requirements for the ETS are described using a functional decomposition method. This is where requirements are successively broken down into simpler requirements and the relationships between requirements are captured in a graphic form. The requirements are written as the transformation of inputs into outputs, resulting in a model of the total system.

Each lowest level requirement is then allocated to one of four functional groups (FG) shown in Figure 2. These groups illustrate the variations of the three different system architectures, as the functions they represent will be accomplished either on an EV or within the EVSE, depending on the architecture. Physical requirements for the channels used to transfer the power and communicate information between the EV and the EVSE are then defined as a function of architecture. System architecture variations are referred to as follows:

Type A—Conductive AC System Architecture—Section 7.2.1

Type B—Inductive System Architecture—

Type C—Conductive DC System Architecture—Section 7.2.3

The requirements model in Section 6 is not intended to dictate a specific design or physical implementation, but rather to provide a functional description of the system’s expected operational results. These results can be compared against the operation of any specific design. Validation against this document is only appropriate at the physical boundary between the EVSE and EV.

SAE J2293/2

SAE Recommended Practice for Energy Transfer System for Electric Vehicles Part 2: Communication Requirements and Network Architecture

See part 1 but for communications and networking. Stabilized 2014, intended to be a historical document (same as part 1).

Power Distribution Equipment Requirements for EVSE

The integration of EV charging supply equipment requires the integration of several high-power loads and an adaptation to the existing electrical infrastructure. This section presents basic principles for designing the EV charging infrastructure and its integration into an existing electrical installation.

For more information on power distribution equipment options, please see the Power Distribution Equipment section of this design guide. For EVSE applications, the focus will be on low voltage equipment: panelboards, switchboards, and dry-type transformers.

The first consideration for power distribution equipment is how the EVSE will get their power.

Different charging levels require different power distribution equipment.

Level 1

Level 2

Level 3

Level 2 and 3

Large Installations

Utility metering required, unless fed from internal facility feeder.

Megawatt Charging

One promising architecture for extra-large megawatt charging applications is to utilize a solid state transformer with a medium voltage AC input and a DC output for power distribution to the MW dispenser(s).

EV Charger Applications

Common use cases:

  Residential Multifamily Fleet Charging
Typical use case Single-family homes (residential and/or commercial contractors) Housing complexes that serve multiple families with dedicated or shared charging Centralized depot charging for fleet vehicles (light-duty or medium-duty)
Power requirement ≤19.2 kW (AC Level 2) ≤19.2 kW (AC Level 2) DCFC and/or AC Level 2
EV charger Schneider Charge Pro AC Schneider Charge Pro AC DCFC and/or Schneider Charge Pro AC
Power distribution Square D Energy Center
OR
Schneider Pulse
OR
QO Load Center
QED2 Switchboard
FlexSeT Switchboards
IPC2 EV Pod
NQ Panelboard
EZM Metering
QED2 Switchboard
IPC2 EV Pod
LV Transformer
NQ Panelboard
For larger installations:
MV Switchgear
MV Distribution Transformers
LV Switchgear or Switchboards
ECC for DERs
BESS
Software Schneider Home EV Connect Multifamily Software EV Connect Energy Fleet Management
  At Work Destination In Transit
Typical use case Corporate or commercial EV charging sites where commuters park their EVs while at work Public, non-DCFC charging sites where people spend an extended time Public DCFC sites, such as gas stations, convenience stores, etc.
Power requirement ≤19.2 kW (AC Level 2) ≤19.2 kW (AC Level 2) ≥150 kW DCFC
EV charger Schneider Charge Pro AC Schneider Charge Pro AC ≥150 kW DCFC
Power distribution QED2 Switchboard
FlexSeT Switchboards
IPC2 EV Pod
NQ Panelboard
LV Transformer
QED2 Switchboard
FlexSeT Switchboards
IPC2 EV Pod
NQ Panelboard
LV Transformer
QED2 Switchboard
IPC2 EV Pod
LV Transformer
NQ Panelboard
For larger installations:
MV Switchgear
MV Distribution Transformers
LV Switchgear or Switchboards
ECC for DERs
BESS
Software EV Connect Energy Management
EcoStruxure Energy Hub
EcoStruxure Power
EV Connect Multifamily Software EV Connect Network
EcoStruxure Energy Hub

Scenario 1: A power system study has determined that there is sufficient capacity in the existing system to add the EVSE specified for the site.

If the number of charging points and their capacity is significantly lower than the installed power, an option to investigate could be to integrate the EV chargers into the existing electrical installation, as shown in the following.

EV Loads Integrated into the Existing Electrical Infrastructure

It is important to perform a power system study to ensure the power load can be added to the existing electrical infrastructure. Energy efficiency measures could be proposed to reduce the existing consumption and therefore increase the power demand that can be added. Local power supplies and storage could be proposed to compensate for the impact of integrating the EV charging equipment. If the existing LV switchboard cannot accommodate the additional power and/or devices required, the option described in next paragraph is recommended.

As specified in NEC Section 625, the power distribution equipment feeding the EVSE shall have sufficient rating to supply the load served. Overcurrent protection for feeders and branch circuits supplying electric vehicle supply equipment shall be sized for continuous duty and shall have a rating of not less than 125 percent of the maximum load of the electric vehicle supply equipment. Electric vehicle charging loads shall be considered continuous loads unless an automatic load management system is used, in which case the maximum equipment load on a service and feeder shall be the maximum load permitted by the automatic load management system. This section assumes that an automatic load management system is not present. More information about automatic load management systems and smart charging may be found in the Charge Management Software section.

Municipal guidelines should be consulted for new construction projects involving parking to determine the minimum number of spaces that need EVSE. Some utilities offer special rates for EV charging installations. To be eligible for the EV tariff, utility requirements may specify a dedicated meter for the EV chargers.

Remembering charger types:

  • AC Level 2 chargers are typically rated for installation in 208/120 V systems or 240 V systems. Most require a 2P breaker as OCPD.

  • DCFC will typically be fed from a 480 V 3P breaker.

For example, consider a site with (10) Level 2 chargers rated 7.2 kW / 30 A. For each breaker rating, find 125% of the EVSE’s current rating:

30 A * 1.25 = 37.5 A

The OCPD for each of the chargers will be the next highest available standard size: 40 A.

A 208/120 V panelboard to feed these (10) chargers may have a panel schedule like this:

CKT # Load Desc. Trip Pole A B C Pole Trip Load Desc. CKT #
L BUS R BUS L BUS R BUS L BUS R BUS
1 7.2 kW Charger 40 A 2 3120 3120         2 40 A 7.2 kW Charger 2
3     3120 3120    
5 7.2 kW Charger 40 A 2         3120 3120 2 40 A 7.2 kW Charger 2
7 3120 3120        
9 7.2 kW Charger 40 A 2     3120 3120     2 40 A 7.2 kW Charger 2
11         3120 3120
13 7.2 kW Charger 40 A 2 3120 3120         2 40 A 7.2 kW Charger 2
15     3120 3120    
17 7.2 kW Charger 40 A 2             2 40 A 7.2 kW Charger 2
19 3120 3120        
21                          
23            
25                          
27            
29                          
    Total Load (VA): 24960 18720 18720        

The total connected load is 62400 VA, or 173.2 A. The next highest main breaker size would be 200 A.

Schneider Electric NQ Panelboard

Schneider Electric NQ Panelboards have 400 A and 600 A options with main circuit breakers. These panels can be applied at 208 V or 240 V, either alone or in an IPC2 unit. If more Level 2 chargers are required, they may be fed from additional panels.

The following quantities use a continuous current rating for the EVSE loads (no LMS)

Charger NQ 208 V 400 A NQ 208 V 600 A NQ 240 V 400 A NQ 240 V 600 A
Quantity Quantity Quantity Quantity
7.2 kW L2 18 26 16 24
7.6 kW L2 17 25 15 22
9.6 kW L2 13 20 12 18
11.5 kW L2 11 17 10 15
19.2 kW L2 6 10 6 9
NOTE: 70 A to 100 A 2P breakers are limited to 11 breakers per panel due to the neutral connection limitations.

IPC2 “EV Pod”

Available Voltage (utility xfmr sec or point in system where to tap off for EVSE addition) Type of EVSE Needed Recommended Equipment
480 V DCFC Chargers Switchboard with breakers to DCFC
OR
Switchboard to I-Line panels to DCFC
480 V AC L2 Chargers 480 V switchboard to step-down transformer to panel(s) to L2 EVSE
OR
480 V switchboard to IPC2 “EV Pod” integrated step-down transformer and panels to L2 EVSE
480 V Mix of DCFC and L2 Chargers IPC2 “EV Pod” with a 480 V panelboard, step-down transformer, and 240 V or 208 V panelboard
208/120 V DCFC Chargers Step-up transformer to 480 V I-Line panelboard or QED2 switchboard
208/120 V AC L2 Chargers NQ Panelboard
208/120 V Mix of DCFC and L2 Chargers IPC2 “EV Pod” with a 208/120 V panelboard, step-up transformer, and 480 V panelboard

IPC2 “EV Pod” elevation with 480 V, 800 A I-Line panelboard, step-down transformer, and 208 V, 600 A NQ panelboard

The Scenario 1 example and variations presented below cover the addition of EVSE to sites with existing power distribution systems. Many existing businesses and sites are retrofitting and/or adding to their existing systems to accommodate the demand for EVSE.

If the power demand of the new EV loads is equivalent to or higher than that of the existing electrical installation, it could be preferable to install a new main LV switchboard to integrate all EV loads. The existing electrical infrastructure will be connected to this new main LV switchboard. A power system study should be performed to ensure overcurrent protective device coordination between the existing installation feeder and the new main incoming device.

If there are several EV chargers located at the same area, secondary LV switchboards or panelboards could be installed close to the EV charging area to minimize the cable length.

The creation of a new main LV switchboard presents the advantage of minimizing the changes to the existing electrical installation. In addition, it offers the opportunity to coordinate protection devices and thus optimize the power availability.

EV Loads Integrated into a New Main Low Voltage Switchboard

The integration of EV loads increases the power demand of the electrical installation significantly. An extension of the local energy infrastructure is often required. A switch from a LV grid connection to a MV grid connection could be necessary in certain cases.

In addition to the electrical infrastructure, the electricity contract with the energy provider needs to be reviewed.

To limit or avoid these types of significant modifications to the existing local installation, local energy power supplies can be added, such as:

  • Photovoltaic system: for local energy production and a commitment to sustainability.

  • Energy storage system: to avoid power demand peaks and optimize solar production use.

  • Combined heat and power (CHP): combined heat and power production if relevant.

Local power supplies can be connected to the new main LV switchboard. Their integration into an existing electrical infrastructure requires a preliminary audit.

EV Loads and Local Power Supplies Integrated into a New Main Low Voltage Switchboard

Busduct

Example solution for a parking structure.

I-Line Busway

800–5000 A busway

Aluminum and/or Copper

Plug-in or bolt-on disconnects

30 A, 60 A, 100 A, 200 A, 400 A, 600 A + plug-in circuit breaker disconnects

Fusible or circuit breaker plug-in units

Circuit breakers with electronic trip unit (ETU), communications (Ethernet or Modbus)

Charge Management Software

Charge Management Software (CMS) communicates directly with the EV chargers for monitoring and control. Automatic load management systems can alleviate the impact of EV installations by setting a maximum power limit for a group of EVSE. This software is also how equipment owners can bill for charger usage and drive ROI on their EVSE investment.

Key terms:

  • Smart chargers are internet enabled hardware units that work with software management to provide the best driver and owner experience. Smart chargers are also required hardware when applying for incentives.

  • Software management enables you and your clients to have complete control of your charging program, reduce costs, capture incentives, and ensure a positive ROI and driver experience.

  • Load Management Software balances the existing output capability among the energy-consuming assets in a building or business. Linked directly to a site’s electrical capacity. Works with smart charging and demand response.

  • Demand Response is implemented at the power company level.

As illustrated in the following, there are different communication protocols between the electric vehicle (EV) and the electric vehicle supply equipment (EVSE), and between the EVSE and the CMS.

ISO 15118 is a set of protocols that allow EVs to communicate with charging stations. ISO 15118-2 pertains to network and application protocol requirements for communication between electric vehicles and charging stations.

  • Plug & Charge – A standardized, secure authentication process where an EV automatically identifies itself to the charging station, initiating and authorizing charging without requiring user interaction (such as RFID cards or apps).​

  • AutoCharge – A simpler method for automatic charging session initiation based on the vehicle’s MAC address. AutoCharge starts charging when the vehicle is recognized by the charging station.

Feature Plug and Charge AutoCharge for Level 2
Communication ISO 15118–2 ISO 15118–2
Standard ISO 15118 Proprietary (no universal standard)
Security High (uses encrypted certificates) Moderate
Setup Complex (requires EV, charger, and CPO support) Simple (requires MAC address registration)
Vehicle Requirement ISO 15118 compliant vehicles ISO 15118 compliant vehicles
Primary Use Case Public charging, fleets Commercial fleets

Open Charge Point Protocol (OCPP) is an open communication protocol that allows EV charging stations to communicate with central management systems. There are several versions currently available and in development.

  • OCPP 1.6 – Widely used, supports basic smart charging and device management.​

  • OCPP 2.0.1 – Introduces enhanced security, plug-and-charge, and better support for energy management.​

  • OCPP 2.1 – Vehicle-to-grid (V2G) support.

Feature OCPP 1.6 OCPP 2.0.1 OCPP 2.1
Security Standard Advanced Further Refined
Smart Charging Device Level Control Hierarchical Control V2G
Diagnostics Limited Improved Enhanced
Plug and Charge Yes Yes Yes
V2G Support No Limited Yes
Compatibility Not Compatible with 2.0.1 or 2.1 Compatible with 2.1 but not 1.6 Compatible with 2.0.1 but not 1.6

It is important to specify the correct OCPP firmware revision on the charger to ensure that the desired EVSE and CMS are compatible. Typical language may read, “must support OCPP 1.6J or later with smart charging profiles. To ensure compatibility, charger must undergo certification testing with EVConnect.”

Smart chargers must be able to communicate via internet, wired or wireless, and support web socket communication. Commonly specified communications capabilities are WiFi 802.11 at 2.4 GHz for wireless network communication, Ethernet 10/100, and 4G LTE Cellular connectivity with a sim card that may or may not be swappable in the field. Some users prefer to also specify EVSE that is capable of a local list support or freevend offline/non-network mode fallback configuration.

Cybersecurity is an important consideration with any connected product. One way to ensure safety when specifying a smart charger is to specify that the EVSE must include a trusted platform module (TPM) developed using an IEC 62443 compliant reference framework for cybersecurity.

In order to provide accurate data to the CMS, the EVSE should include an imbedded submeter for measurement and reporting of electricity delivered to the EVSE. ±1% accuracy is a commonly specified value for the internal meter.

There are extensive possibilities for monitoring, control, and logging with charge management software. Commonly specified features include remote monitoring and control, cost calculations, and charge history. Knowing what you can manage and how is key to helping your clients understand why software management is necessary with their EV charging program if full ownership of the solution with complete visibility and control is desired.

There are many ways you and/or your clients may want to manage charging. You may want to manage unique driver groups differently, encourage increased utilization by implementing overstay fees, know when it is time to add more stations because the current allotment is being fully used, or address issues quickly to optimize the driver experience.

You will also want to bill drivers correctly for the energy they use and save money by managing on and off-peak energy utilization. Many energy providers charge you significantly more according to the peak amount you consume in a given time period. As such, doing things that spike the site’s load will cause a jump in the bill.

Managing all of this can sound daunting, but it does not need to be. You can provide a solution that does not take hours and hours each week to monitor and adjust. A good software management platform will enable you to set it up, track progress, understand utilization, view revenue, and track key metrics you and/or your clients need for reporting in a simple, easy to understand dashboard.

The management system will need to enable your EV charging program to operate within your site’s current electrical capacity and with your local energy provider’s capacity, not against it.

The electric grid is fragile and as climate change increases, we are seeing more failures. How will a shift to electric vehicles affect this? In 2019, Americans drove roughly 9 billion miles per day. A “high efficiency” electric vehicle gets about 4 miles per kilowatt-hour. So, that is an average nationwide daily energy use of 2.25 billion kilowatt-hours. Meanwhile, nationwide energy use comes to about 10.6 billion kilowatt-hours per day. In other words, EVs would up demand on the grid by 20%.

Moreover, vehicle charging is more difficult to manage. The grid needs to be able to “predict” high demand times to stay stable. An additional 2.25 billion kilowatt-hours of consumption spread across people’s varied schedules creates substantial difficulty.

Demand pricing and grid balancing are about when electricity is consumed, along with how much is consumed. Demand will go up with electric vehicles, so load management focuses on controlling the “when.” But load management systems also take on another issue: distribution of electricity through all EVs plugged into a system.

By managing these two variables in tandem, load management systems reduce costs for the person using them and protect the local grid, all by managing when electricity is consumed, how much is used and where those amounts go. The ability to manage how much power is being used is critical in minimizing grid failures and optimizing a positive driver experience.

Load management ensures clients avoid costly infrastructure and services upgrades by managing how much electricity they need to bring to their panel to power their chargers. This is critical for setting yourself and clients up for a shorter ROI.

Let us say there is a need for 30 chargers, but only enough room on the panel for 6. Load management will enable you install all 30 chargers by oversubscribing the panel without fear of going over electrical limits. You and your clients can avoid service upgrades, new transformers, panel upgrades or replacements, etc., saving 10’s or 100’s of thousands of dollars and streamlining the project timeline. This also makes your bids more competitive than others who do not have a firm grasp of this concept.

Load management systems operate in different ways. Most focus on three qualities: controlling when electricity is used, where it goes and how much goes to each vehicle, all with minimal effort on the part of the user.

Types of Load Limits: EV Connect supports both current and power limits in setting charging profiles.

  • Current Limit (A): Limiting the maximum amperage of a group of stations based on the size of the upstream circuit breaker or panel.

  • Power Limit (kW): Limiting the maximum power (kW) of a group of stations served by one transformer.

  • Some sites are also subject a utility rate that requires aggregate load stay below a power threshold.

Load Balancing Logic: Load is balanced in near real time using two mechanisms: Proportional or Fleet.

  • Proportional Load Sharing - Each active session is provided a proportional percentage of the available power limit, scaled by the rated capacity of charging stations.

In general, a client will be able to prioritize different elements. For instance, you can prioritize reducing energy cost by instructing the system to charge vehicles separately throughout the night, with a maximum consumption limit. This allows you to ensure that each vehicle is charged as much as possible without threatening the electrical grid or risking high demand charges. Some can even be programmed to consume more electricity when the grid has more capacity than demand, allowing users to make use of that gap while assisting the electrical grid.

Using the example above, let us say your client has all 30 chargers installed off 6 circuits – each with capacity for 1 charger. When driver 1 plugs in, they will get 100% of the power. When driver 2 plugs in, both cars will get 50%. When driver 3 plugs in, all three get 33%, and so on for each circuit. Ideal for scenarios where drivers are parked for long duration, you can see how this has a positive impact on your client’s infrastructure costs and charging capacity.

These systems are remarkably simple to use, too. You select peak power or energy usage and tell the system how to judge that amount: either by the total amount consumed or amount used over a specific period of time or make the amount responsive to grid demand. You then set power-sharing settings, picking certain amounts for each vehicle, or using a first-in, first-out system.

Here’s how load management uses software to maximize the site’s current infrastructure:

If such solution is not installed, the installation should be sized for the maximum power demand without considering charging period and usage coefficient. As consequence, the installation will be oversized versus the real need, and the costs of the EV charging infrastructure will be higher.

So, as you can see, without software, you cannot design an optimal charging program, and therefore cannot maximize a charging program for yourself or a client. ROI is contingent on reducing your up-front infrastructure costs, capturing incentives, managing pricing or time of use, enabling driver groups, and billing them accurately, tracking utilization, increasing uptime, and operating within the grid capacity you have.

With software, all of this is possible. With EV Connect, all of this easy.

By partnering with EV Connect, you are choosing a partner who empowers you to power your client’s EV charging programs. We put you in the driver’s seat to build, manage, service, track and grow the right solution for your clients and prospects. We understand that your success is directly tied to your ability to easily provide competitive quotes, limit time needed to set-up, service and manage chargers, and be the expert your clients are looking to when they want to offer EV charging.

While there are basic power management software platforms for any building site, it makes the most sense to communicate with the experts at EV Connect to discuss your power management needs. Working in tandem with demand response from the power company, smart charging, software management and power management have the potential to significantly reduce your site costs. Not to mention this helps ensure a sustainable future for EVs if sites can continue to maximize the potential of their existing power infrastructure.

Sources

  1. Energuide.BE – Why Does the Electrical Grid Have To Stay in Balance?

  2. Kelly Blue Book – Average Miles Driven Per Year: Why It’s Important

  3. Select Car Leasing – Miles Per KwH - The New MPG

  4. Energy Information Administration (EIA) – Electricity Consumption in the United States Was About 3.9 Trillion Kilowatthours (kWh) in 2021

  5. Schneider Electric – What Is a Power Management System, and How Does It Help Optimize Uptime and Efficiency?

  6. EnergyStar.Gov – Activating Power Management: Commercial Software Packages

  7. Environmental Leader – Electric Vehicle Charging Generating Growth in Building Energy Management Systems

  8. McKinsey – Charging electric-vehicle fleets: How to seize the emerging opportunity

Bidirectional Charging

Bidirectional Charging refers to systems that are capable of power flow in two directions: the power to charge the battery in an electric vehicle, as discussed earlier in this section, and reverse power flow from the electric vehicle battery back to the rest of the system. Bidirectional charging requires an EV capable of reverse power flow, EVSE capable of bidirectional power flow, and software to communicate with and manage all the components.

ISO 15118-20 is the ISO 15118 standards document that pertains to vehicle to grid communication standards.

Bidirectional charging is sometimes referred to as V2X or “vehicle to everything” charging. There are also specific types of bidirectional charging discussed in the following.

  • Vehicle to grid (V2G): Through a converter that is usually present in the charger, vehicles can send energy directly back to the grid. This can facilitate more energy efficiency for a local power grid and lead to cost savings by enabling charger owners to get paid for helping maintain grid reliability.

  • Vehicle to home (V2H): Bidirectional V2H charging turns a car battery into a backup power source for a home. This also allows for more efficient energy usage and potential cost savings and typically relies on technology that is built into the charger.

  • Vehicle to load (V2L): The EV battery can be used to power appliances and tools on the go. This type of charging relies on vehicles that have built-in converters and 120-volt plugs for charging appliances and devices.

  • Vehicle to vehicle (V2V): A specific application of V2L charging where the load is another electric vehicle. V2L allows the transfer of energy from one car to another.

By creating this two-way energy stream, bidirectional charging offers several benefits to EV owners, both in terms of potential savings and energy efficiency.

  1. Save Money on Energy Use

    Bidirectional charging unlocks potential savings for vehicle owners in two ways. First, smart-charging technology, coupled with bidirectional charging, can turn a car into an efficient power source for a home or business. The vehicle charging can be set to charge during off-peak hours or when renewable sources are available.

    Second, with vehicle-to-grid technology, you can sell energy back to the utility company for redistribution. This can further reduce your utility costs. One study by the University of Rochester found that V2G chargers can save EV owners $120 to $150 per year.

  2. Store Backup Power for Your Home or Business

    Beyond cost savings, bidirectional charging can also provide peace of mind for homeowners and business owners. If you are caught in a power outage, V2H charging allows your vehicle to serve as a backup power source while the utility company conducts repairs. The typical electric car battery holds about 60 kilowatt-hours of electricity, which is enough to power a home for roughly two days.

  3. Create a Portable Power Source

    Thanks to bidirectional technology, in some cases, that same battery that can power your home can also go on the road with you to serve as a mobile power source. If you take your EV camping or out on the job, for instance, you can use it to power appliances. In a pinch, you could even use it to provide energy for someone else’s car.

Sources:

  1. Autotrends – What Is Bidirectional Charging?

  2. University of Rochester – Can Electric Cars Help Strengthen Electrical Grids?

  3. World Resources Institute – How California Can Use Electric Vehicles To Keep the Lights On

  4. Clean Energy Reviews – Bidirectional Chargers Explained - V2G Vs V2H Vs V2L

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.