0100DB2301

Power Quality Considerations

Abstract: Power system health is paramount to the longevity of power distribution system equipment and the reliability of continuous power. Power quality affects distribution equipment, as well as downstream process level equipment and loads. It is vital that power quality is considered in the design of a system as well as allowing for monitoring functionality after the equipment is installed and commissioned to monitor health, troubleshoot issues, and capture issues and occurrences.

Introduction

The term power quality may take on any one of several definitions. The strict definition of power quality is “the concept of powering and grounding electronic equipment in a manner that is suitable to the operation of that equipment and compatible with the premises wiring system and other connected equipment” (see IEEE Recommended Practice for Powering and Grounding Electronic Equipment*). In practice, however, the term power quality is often used to denote the proximity of the system voltage to its sinusoidal form at the nominal voltage level. Deviation from this sinusoidal norm therefore denotes a power quality issue. Strictly speaking, this deviation is a power disturbance, defined as “any deviation from the nominal value (or from some selected thresholds based upon tolerance) of the AC input power characteristics” IEEE Recommended Practice for Powering and Grounding Electronic Equipment*. The most common power disturbances are, as defined by IEEE Recommended Practice for Powering and Grounding Electronic Equipment*:

Overvoltage: An RMS increase in the AC voltage, at the power frequency, for a period of time greater than one minute. Typical values are 110% - 120% of nominal.

Undervoltage: An RMS decrease in the AC voltage, at the power frequency, for a period of time greater than one minute. Typical values are 80 – 90% of nominal.

Swell: An increase in RMS voltage or current at the power frequency for durations from .5 cycle – one minute. Typical values are 110% - 180% of nominal.

Sag: An RMS reduction in the AC voltage, at the power frequency, for durations from ½ cycle to a few seconds.

Interruption: The complete loss of voltage. A momentary Interruption is a voltage loss (<10% of nominal) for a time period between .5 cycles and three seconds). A temporary interruption is a voltage loss (<10% of nominal) for a time period between three seconds and one minute. A sustained interruption is the complete loss of voltage for a time period greater than one minute.

Notch: A switching (or other) disturbance of the normal power system voltage waveform, lasting less than ½ cycle; which is initially of opposite polarity to the waveform, and is thus subtractive from the normal waveform in terms of the peak value of the disturbance voltage. This includes a complete loss of voltage for up to ½ cycle.

Transient: A subcycle disturbance in the AC waveform that is evidenced by a sharp discontinuity of the waveform. It may be of either polarity and may be additive to, or subtractive from, the nominal waveform.

Flicker: A variation in input voltage, either magnitude or frequency, sufficient in duration to allow visual observation of a change in electric light source intensity.

Harmonic Distortion: The mathematical representation of distortion of the pure sine waveform. This refers to the distortion of the voltage and/or current waveform, due to the flow of non-sinusoidal currents.

Electrical Noise: Unwanted electrical signals that produce undesirable effects in the circuits of the control systems in which they occur. Noise may be further categorized as transverse-mode noise, which is measurable between phase conductors but not phase-to-ground, and common-mode noise, which is measurable phase-to-ground but not between phase conductors. This noise may be conducted or radiated. Also referred to as RFI (radio-frequency interference) or EMI (electro-magnetic interference).

The causes of the common power disturbances listed can vary greatly. Common causes are listed in Common Power Disturbance Causes.

Common Power Disturbance Causes

Disturbance

Common Causes

Overvoltage

Voltage regulator malfunction

Improperly set transformer taps

Improperly applied power factor correction capacitors

Undervoltage

Voltage regulator malfunction

Improperly set transformer taps

Large source impedance (“weak” system)

Voltage swell

Recovery of system voltage following a fault

Remote switching (capacitors, etc.)

Voltage sag

Remote fault

Cold-load pickup (motor starting, transformer energization.)

Large step loads

Transient (Typically voltage surges)

Lightning strikes

Close-in switching (capacitors,)

Complex circuit phenomena such as current chopping, restrikes, system resonance.

Flicker

Arcing Loads such as arc furnaces

Also, same sources that cause voltage sags and swells

Notches and harmonic distortion

Power electronic converter equipment such as rectifiers, inverters, drives, which produce non-sinusoidal load current and commutation notches

Interruptions

Faults causing overcurrent protective device operation

Utility maintenance activities

Electrical noise

Power Electronic converter equipment such as drives

Conductors and power equipment which carry large amounts of current

Arcing in overcurrent protective devices

Power disturbances can greatly affect utilization equipment. For example, sensitive electronic medical equipment can malfunction, adjustable speed motor drives may trip off-line. Interruptions can cause microprocessor-based equipment such as computers to lose data. In extreme conditions, such as for voltage surges caused by direct lightning strikes, both power equipment and utilization equipment may be subject to stop functioning. With the high reliability requirements imposed upon power systems, it is imperative that power system disturbances, or potential disturbances, be mitigated to avoid down-time, equipment loss, and risk to human life.

Power Quality Metrics

There are various methods for categorizing the severity of power disturbances. The most typical indices for measuring power quality disturbances are:

Distortion Factor: The ratio of the root square value of the harmonic content to the root square value of the fundamental quantity, expressed as a percentage of the fundamental, also known as total harmonic distortion *.

(13–1)

Where:

  • Vh is the RMS harmonic voltage (or current) value at a frequency of n times the fundamental frequency.

  • V1 is the RMS fundamental-frequency voltage or current.

Alternate forms for the distortion factor are given in IEEE Recommended Practices and Requirements for Harmonic Control in Electrical Power Systems* as percentages of the nominal voltage or demand load current for the system under consideration, for use in evaluation of the harmonic content of the system voltage or current. These are referred to as Total Harmonic Distortion (THDVn) and Total Demand Distortion (TDD), defined as follows:

Where:

  • Vh is the RMS value of the nth harmonic component of the voltage.

  • Vn is the RMS nominal fundamental voltage value.

  • Ih is the RMS value of the nth.

  • IL is the maximum demand load current, typically the average maximum monthly demand over a 12-month period.

Crest Factor: The ratio of the peak value of a periodic function to the RMS value, that is:

Crest factor (cf) = ypeak/yrms

(13–4)

Where:

  • Ypeak is the peak value of a periodic function.

  • Yrms is the RMS value of the function.

Because power system voltages and currents are nominally sinusoidal, the nominal crest factor for these would be √2 , which is 1.414 (see Electric Power Fundamentals for details).

Notch Area: A notch in the power system voltage (or current) is illustrated in Common Power Disturbance Causes IEEE Recommended Practices and Requirements for Harmonic Control in Electrical Power Systems*:

Voltage (or Current) Notch Illustration

The notch area for the notch as illustrated in Common Power Disturbance Causes is defined as:

an = t x d


(13–5)

Where:

  • An is the notch area in volt-microseconds.

  • t is the notch time duration in microseconds.

  • d is the notch depth in Volts.

Recovery Time: This is the time needed for the output voltage or current to return to a value within the regulation specification after a step load or line change.

Displacement Power Factor: The ratio of the active power of the fundamental wave, in Watts, to the apparent power of the fundamental wave, in VA. This is the traditional definition of power factor.

Total Power Factor: The ratio of the total input power, in watts, to the total VA input. This includes the effects of harmonics.

K Factor: A measure of a transformer’s ability to serve non-sinusoidal loads. The K factor is defined as:

(13–6)

Where:

  • Ih is the harmonic component at h times the fundamental frequency.

  • h is the harmonic order of Ih in multiples of the fundamental frequency.

  • hmax is maximum harmonic order present.

Voltage Surges

The causes of voltage surges may be split into two major categories: Power system switching and environmental (see IEEE Recommended Practice for Powering and Grounding Electronic Equipment*). Both exhibit decaying oscillatory transients. Capacitor switching close to the point under consideration is the most common cause of switching surges, while lightning is the most common cause of environmentally-induced voltage surges. Both can cause severe damage to unprotected power system components, with the potential for lightning damage being the most severe; in the worst case, lightning damage can be catastrophic.

Surge arrestors, as described in System Protection, are typically used to minimize voltage surges. On low-voltage systems surge protective devices (SPD), also described in System Protection are also used. For motors, surge capacitors are an option. In severe cases, custom-designed R-C snubber circuits may be required as well.

Voltage Sags, Swells and Interruptions

Voltage sags, swells and interruptions have many causes. Remote switching or lightning strikes can cause voltage swells, as can the recovery of the system voltage after a fault. Voltage sags can be caused due to transformer or motor inrush or large step loads, especially on systems without large amounts of available fault current. Voltage interruptions are generally caused due to protective device operation.

Protection of sensitive equipment against voltage sags and swells can be difficult. Fast-acting voltage regulators offer one means of defense against these phenomena, although any voltage regulator must be properly applied to avoid worsening the problem. Fast-acting voltage regulators can generally be classified as tap-switching, buck-boost, or ferroresonant (also known as CVT “constant voltage transformer”) types (see IEEE Recommended Practice for Powering and Grounding Electronic Equipment*). New solid-state tap switching technologies for voltage regulators provide faster response than older, electromechanical switching technologies. Other devices, such as “power line conditioners” which combine some TVSS functions with voltage regulation and noise reduction, and motor-generator sets, are also used (see IEEE Recommended Practice for Powering and Grounding Electronic Equipment*).

Protection of sensitive loads against voltage interruptions is efficiently performed with an uninterruptible power supply or UPS. This device is available in several different topologies and is crucial where microprocessor-based devices are to be powered. UPS discussed in more detail in Emergency Power Distribution Equipment.

Harmonic Distortion

Harmonic distortion is a subject of great interest in modern power systems. Harmonic distortion results from non-sinusoidal load currents. These currents are the result of non-linear loads, such as drives, which employ power electronic devices to rectify the AC waveform. These devices draw non-sinusoidal currents which, in turn, cause non-linear voltages to be developed in the system.

IEEE Standard 519-1992 IEEE Recommended Practices and Requirements for Harmonic Control in Electrical Power Systems* gives recommended limits for current distortion due to consumer loads and voltage distortion in the utility supply voltage. Both are referenced at the point on the utility system where multiple customers can be served, referred to as the Point of Common Coupling (PCC). The requirements from IEEE Recommended Practices and Requirements for Harmonic Control in Electrical Power Systems* for current distortion limits on general distribution systems 120 V – 69 kV are given in . IEEE 519-1992 Harmonic Voltage Distortion Limits shows the corresponding utility voltage distortion limits.

The current limits are given both as limits on the individual harmonic levels and a limit on the TDD, and that as the ratio Isc/IL increases the limits also increase. The reason for this is that the current distortion limits are designed to limit the voltage distortion at the PCC, and the voltage distortion for a given current distortion worsens with a larger source impedance (V̄ = Ī  • Z̄)

IEEE 519-1992 Harmonic Current Distortion Limits for General Distribution Systems 120 V Through 69 kV

Maximum Harmonic Current Distortion in Percent of IL

Individual Harmonic Order (Odd Harmonics)

Lsc/IL

<11

11<h<17

17≤h<23

23≤h<35

35≤h

TDD

<20*

4.0

2.0

01.5

0.6

0.3

5.0

20<50

7.0

3.5

2.5

1.0

0.5

8.0

50<100

10.0

4.5

4.0

1.5

0.7

12.0

100<1000

12.0

5.5

5.0

2.0

1.0

15.0

>1000

15.0

7.0

6.0

2.5

1.4

20.0

Even harmonics are limited to 25% of the odd harmonic limits above.

Current distortions that result in a DC offset, half-wave converters, are not allowed.

*All power generation equipment is limited to these values of current distortion, regardless of actual L SC /IL.

Where:

ISC = maximum short-circuit current at PCC

IL = maximum demand load current (fundamental frequency component) at PCC

IEEE Recommended Practices and Requirements for Harmonic Control in Electrical Power Systems*

IEEE 519-1992 Harmonic Voltage Distortion Limits

Bus Voltage at PCC

Individual Voltage Distortion

(%)

THDVn

(%)

69 kV and below

3.0

5.0

69.001 through 161 kV

1.5

2.5

161.001 kV and above

1.0

1.5

NOTE: High-voltage systems can have up to 2.0% THD where the cause is an HVDC terminal that attenuates by the time it is tapped for a user.

IEEE Recommended Practices and Requirements for Harmonic Control in Electrical Power Systems, IEEE Std*

Mitigation of harmonic distortion is generally accomplished by one of the following means:

  • Passive tuned filters

  • Use of phase multiplication on power conversion equipment

Passive tuned filters are simple series L-C filters. A single tuned passive filter can effectively mitigate one harmonic frequency. They are generally tuned to a value below the harmonic frequency to be attenuated to avoid a resonance condition at that frequency. These are custom-engineered solutions that must be designed specifically for the circuit in question. Passive filters are also used for power factor correction. However, there is a limit to their effectiveness and if higher-order harmonics must be attenuated their use is generally not cost-effective. Take care in all cases to balance the harmonic and power factor correction considerations.

Phase multiplication operates on the principle that if m six-pulse rectifiers are shifted 60/m degrees from each other, are controlled by the same delay angle, and are loaded equally, the only harmonics present are:

h = kq ± 1 (13–7)

Where:

  • h is a harmonic order present.

  • q = 6m and is known as the pulse number of the circuit.

  • k is any integer.

Thus, for standard six-pulse rectifiers the harmonic orders present are 5, 7, 11, 13,…. 18-pulse rectifiers are the current state-of-the-art; for an 18-pulse rectifier (m = 3), the harmonic orders present are 17, 19, 35, 37, …,. For an 18-pulse converter, the lower-order harmonics are thus eliminated. For systems with large numbers of phase-multiplied converters the harmonic current limits in NFPA Emergency Power System Levels are increased by the factor (q/6)1/2, where q is the pulse-number of the predominate non-linear load on the system. In this case the limits for the harmonic orders that do not fit equation (11-7) for the q of the predominate non-linear load are multiplied by a factor of 0.25. Phase-shifting transformer connections are used to achieve the 60/m degree phase shift between six-pulse rectifier units.

Active Harmonic Filters (AHF) can help greatly reduce harmonics and bring systems in compliance with IEEE-519 or other harmonic limits imposed by the utility companies. Current state-of-the-art designs measure the current, filter out the fundamental frequency of the measured current, and inject current that is the negative of the result into the system to cancel the harmonics up to a given harmonic order. These systems are generally used in existing installations that have existing six-pulse drives where replacing the drives is not a cost-effective solution, or where multiple smaller six-pulse drives are utilized since phase multiplication for a drive below 100 HP is generally not cost-effective. State-of-the-art units can also dynamically correct the power factor as well as phase imbalance and are advantageous vs. passive filters both in their effectiveness and their flexibility in power factor correction.

Active Harmonic Filters

Power Quality Monitoring

Power quality monitoring is vital when sensitive equipment or processes are to be powered, and for the overall reliability of the system. Microprocessor-based technology allows the most common power-quality instrumentation to be combined into a single monitoring device which incorporates waveform capture, measures of the power quality metric values per the above discussion, and conventional current, voltage, power, and energy measurements, with minimum/maximum logging capabilities. These devices are typically true RMS-reading instruments, with measurements up to a given harmonic (typically 31st harmonic or higher). The capabilities and sampling rate of the PQ meter must be matched to the sensitivity of the equipment that is being monitored. Not all PQ meters have the required sampling rate to capture fast transients.

Another important consideration is the Disturbance Direction Detection feature that is available in some PQ meters. This feature allows facility staff to quickly pinpoint and isolate the source of the PQ problem and rapidly recover from a potential outage. Refer to the image below.

Power Quality Monitoring

In most cases, a power quality centric EPMS (Energy & Power Monitoring Software) is required to analyze the waveforms, timestamps, sequence of events, etc. to realize a cohesive view of the power quality issues in a facility. Refer to Electrical Energy Management for more details.

The inclusion of power monitoring equipment in the initial power system design makes diagnosis of any subsequent power quality issues, if they arise, much easier and more efficient. Reference IEEE Recommended Practice for Monitoring Electric Power Quality* contains much information on power quality monitoring and should be consulted for further reference.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.