0515CT2101

Circuit Breaker Selection

Select a catalog number from the preceding table.

For special applications, modify the catalog number as follows:
E D B 3 4 0 7 0 _ _ _ _ _ _ _ _ _ _

Factory Installed Options *
Option Meaning Example:
AABA 1A1B Aux. Switch, Normally-open Alarm Switch Package To order a three-pole 480Y / 277 Vac 70 A “D” interrupting rating level circuit breaker with factory-installed copper lugs and an auxiliary switch and alarm switch package:

EDB34070AABALC

AABASA 1A1B Aux. Switch, Normally-open Alarm Switch, 120 Vac Shunt Trip Package
SA 120 Vac Shunt Trip Package
CA Special Ambient Temperature: 122°F (50°C) (Not UL, CSA, or NOM Certified)
LC Copper Lugs
LH High Ampere Standard Lugs
     
  EDB24030 EDB34125
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.