0515CT2101

Powerlink™ ECB-G3 Circuit Breakers

Remotely Operated Circuit Breakers

Powerlink G3 remotely operated circuit breakers are designed for installation in Schneider Electric NF lighting panelboards as part of the Powerlink G4 Lighting Control System. These circuit breakers provide the same overcurrent protection as found in standard circuit breakers.

  • Robust 24 Vdc motor and trip mechanism provide remote operation capability in terms of compact size, electrical ratings, and mechanical life.

  • Motor and drive train can open and close the contacts when the circuit breaker handle is in the ON position.

  • Contacts cannot be closed remotely when the handle is in the OFF position, or the circuit breaker is tripped.

  • Manual override selector located on the front of the circuit breaker provides bypass of automated control command.

  • In manual mode, the motor drive train is disconnected from the contact, allowing the circuit breaker handle to operate the contacts like a conventional circuit breaker.

  • Remote contact status indication determines the presence or absence of voltage on the load side terminal of the circuit breaker.

Tripping System with RMS Sensing

  • Schneider Electric Powerlink ECB-G3 circuit breakers have a permanent trip unit that contains a factory preset thermal (overload) trip element and a magnetic (short circuit) trip element in each pole.

  • The thermal trip element—true RMS sensing—is calibrated to carry the continuous current rating of the circuit breaker at 140°F (40°C) free air ambient temperature.


ECB-G3 Circuit Breakers

ECB-G3 Circuit Breakers, Bolt-On Remotely Operated

Ampere
Rating

One-Pole
277 Vac – 14,000 AIR
120 Vac – 65,000 AIR
Two-Pole
480Y / 277 Vac – 14,000 AIR
120 / 240 Vac – 65,000 AIR
240 Vac – 14,000 AIR Ground B Phase
Three-Pole
480Y / 277 Vac – 14,000 AIR
240 Vac – 42,000 AIR

15

ECB14015G3

ECB24015G3

ECB34015G3

20

ECB14020G3

ECB24020G3

ECB34020G3

30

ECB14030G3

ECB24030G3

ECB32030G3

ECB-G3 Circuit Breakers for Emergency Lighting (requires two pole spaces)

Ampere Rating

One-Pole 480 Y/277 – 14,000 AIR 240 V – 65,000 AIR

20

ECB142020G3EL

NOTE:

All are listed as HACR type for use with air conditioning, heating and refrigeration equipment having motor group combinations and marked for use with HACR type circuit breakers. UL® listed as HID rated for use with high intensity discharge lighting systems. (1) #10–8 Al or (1) #12–8 Cu. Suitable for use with 167°F (75°C) conductors.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.