1640CT0801

Typical Wiring Diagrams

1-Phase, 3-Wire
100–225 A Main Lugs 150 A Max. Branch Mounted Main Circuit Breaker 15–225 A Main Circuit Breaker Types H-, J-, or Q-Frame
     
400–600 A Main Lugs 400 A Max. Main Circuit Breaker Type LA/ LH Frame  
3-Phase, 4-Wire
100–225 A Main Lugs 150 A Max. Branch Mounted Main Circuit Breaker 15–225 A Main Circuit Breaker Types H-, J-, or Q-Frame
     
400–600 A Main Lugs 400 A Max. Main Circuit Breaker Type LA/LH Frame  

400 or 600 A NQ with PowerPacT L-Frame Main Breaker and Load End Option—Note Position of Neutral
 
     
 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.