3100CT1602

Catalog Number Description

General Duty Switches Catalog Number Description

Number Segment Character Description D 3 2 1 N RB
Type of Switch Fusible L=Light duty              
D=General duty              
Non-Fusible DU=General duty              
Blades–Switch Poles 1 One-pole              
2 Two-poles              
3 Three-poles              
Voltage Rating 1 120 Vac (plug fuse)              
2 240 Vac              
Ampere Rating 1 30 A              
2 60 A              
3 100 A              
4 200 A              
5 400 A              
6 600 A              
7 800 A              
Neutral N Factory-installed neutral (neutrals are field-installed on most general duty safety switches).    
Enclosure No suffix NEMA Type 1              
R NEMA Type 3R              
RB NEMA Type 3R (bolt-on hub provision)    
Factory Modifications* N/A                
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.