46010-522-01

Receiving, Handling, and Storage

Receiving

  1. Check the packing list against the equipment received to ensure the order and shipments are complete. Make claims for shortages or other errors in writing within 30 days after receipt of shipment. Failure to do so constitutes unqualified acceptance and a waiver of all such claims to the purchaser.

  2. Upon receipt, inspect the equipment for damage. If you find or suspect damage, immediately file a claim with the carrier and notify Schneider Electric. Claims for shortages or other errors must be made to Schneider Electric within 30 days after receipt of shipment. Failure to submit a written claim constitutes unqualified acceptance and a waiver of all such claims by the purchaser.

  3. Verify the characteristics indicated on the equipment nameplate, compared to the initial order.

  4. The plastic wrap must be in position on the cubicle and in good condition when it arrives.

Handling

WARNING
top heavy load<span><span><span style="font-family: Arial; ">—</span></span></span>hazard of tipping
  • Stabilize the shipping section with a safety strap to reduce the possibility of tipping.
  • Consult with a certified rigging and lifting expert for any situation not covered in these instructions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

It is recommended that the PremSet switchgear be moved using a forklift truck or an overhead crane. The product ships on a pallet for easy forklift access. For transport and/or positioning, the product must remain packaged and the entire length of the forks must be placed under the product.

WARNING
risk of equipment tipping
To lift and move each section, insert hooks into the provided lifting angles.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Use the hooks to properly lift and move the switchgear. Removable lifting angles are provided for inserting hooks to lift each section. Ensure that the hooks of the lifting gear are placed vertically on the center of the switchgear and that it is balanced.

A

Hooks on angles

B

Lifting cables assembly

C

24 in. (610 mm) minimum from top of switchgear

For dimensions and weights, refer to Dimensions and Weights in bulletin 46010-519-03.

Cleaning and Storage

Cleaning

NOTICE
improper cleaning practices
Follow the cleaning instructions below.
Failure to follow these instructions can result in equipment damage.

If you need to clean the cubicle:

  • Use a sponge and clean water.

  • Do not use alcohol or other solvents.

SOLVENTS AND ALCOHOL FORBIDDEN HIGH-PRESSURE CLEANER FORBIDDEN

Storing

DANGER
hazard of electric shock, explosion, or arc flash
Indoor units must be stored in an environment that does not exceed the defined environmental parameters for storage.
Failure to follow these instructions will result in death or serious injury.

PremSet switchgear should be stored in an indoor climate-controlled space until time of installation. The switchgear is not intended for exposure to high humidity, damaging fumes, steam, salt air, oil vapors, excessive dust, abrasive dust, magnetic or metallic dust, abnormal vibration, shocks, tilting while in storage. Such conditions constitute unusual conditions for service and should also be avoided for storage. Successful performance of standard switchgear applied in unusual environments may require special considerations in developing equipment specifications.

If the equipment is not installed immediately after delivery, it can be stored indoors in a clean, dry, well-ventilated area with a mean temperature of approximately 70°F (21°C).

Monitor the equipment closely in areas with high humidity. If necessary, use a minimum of 100 watts of heat per vertical section to keep the equipment dry during storage. Avoid greasy, smoky heaters that can deposit carbon on insulation, causing tracking and eventual insulation breakdowns.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.