6055CT2201

General Description

Square D by Schneider Electric, offers a new metal-clad switchgear SureSeT that enables end users to digitally control and monitor their medium voltage equipment in a compartmentalized and compact footprint. SureSeT switchgear offers a two-high circuit breaker design in a narrow 26 in. wide footprint and is powered by EvoPacT, our newly designed MV vacuum circuit breaker. SureSeT switchgear is the Smarter, Smaller, and Stronger metal-clad switchgear.

Smarter

  • Embedded sensors enable end users to switch to Proactive Maintenance by providing real-time status of several circuit breaker components.

  • Ability to control and monitor equipment from remote device or local HMI without entering the arc flash zone

  • Circuit Breaker Health Monitoring alerts the user to circuit breaker health, thermal abnormalities, and environmental changes.

  • Product information, records, and project files can be instantly accessed through the Digital Logbook, which is easily accessed by the QR code.

  • Cybersecurity compliant with ISA/IEC 62443 – Levels 1 and 2

  • Available in two-high circuit breaker configuration

Smaller

  • 26 in. wide compact design provides 25% footprint savings compared to conventional metal-clad switchgear.

Stronger

  • EvoPacT MV circuit breaker tested to 30,000 circuit breaker open/close operations and 1,000 circuit breaker racking operations

  • Fully compliant with Metal-clad MV Switchgear ANSI/IEEE standards

  • cULus Listed

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.