7400CT9601R01/23

Stainless Steel Enclosures

Stainless steel enclosures provide better corrosion resistance than standard painted enclosures. Schneider Electric offers an entire line of resin-filled transformers. They are available with 316 stainless steel enclosures to meet demands for extra protection in environments where harsh chemicals or corrosive materials such as acids, food products, gasoline, organic solvents, or salt water are present.

Square D brand transformers with 316 stainless steel have a higher nickel content than 304 stainless steel, making them even more resistant to harsh environments.

Units are painted with standard ANSI 49 gray and have a NEMA Type 3R rating. Additional voltages are available. Contact your local Schneider Electric representative for details. NEMA Type 4X enclosures are also available; contact your local Schneider Electric representative for price and availability.

See Resin Encapsulated Three and Single Phase Transformers for stainless steel options.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.