80043–740–01

Installing the Trim Front

DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, or NOM-029–STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside the equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Local codes vary, but are adopted and enforced to promote safe electrical installations. A permit may be needed to do electrical work, and some codes may require an inspection of the electrical work.
  • Replace all devices, doors and covers before turning ON power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Installing Low Amp Standard Trim

  1. Place the support bracket located at the bottom of the trim front on the enclosure lip, as shown.

  2. Open the trim front door. Align the screw holes in the trim front door recesses with the screw holes in the panelboard deadfront and fasten with the 10-32 x 19/32-in. self-threading screws, included in the kit.

    NOTE: For flush-mounted applications, elevate the interior to the proper position. Refer to the information manual provided with the panelboard for more information.

Installing Low Amp Hinged Trim

  1. Install the spring nuts on the enclosure lip, over the holes corresponding to the screw holes in the trim front.

  2. Place the support bracket located at the bottom of the trim front on the enclosure lip, as shown.


  3. Align screw holes in the trim front with the spring nuts on the enclosure lip and fasten with the 1/4-20 x 1-in. screws, included in the kit.

  4. Open the trim front door. Align the screw holes in the trim front door recesses with the screw holes in the panelboard deadfront and fasten with the 10-32 x 19/32-in. self-threading screws, included in the kit.

    NOTE: For flush-mounted applications, elevate the interior to the proper position. Refer to the information manual provided with the panelboard for more information.

Installing High Amp—Standard or Hinged Trim

  1. Install the spring nuts on the enclosure lip, over the holes corresponding to the screw holes in the trim front.

  2. Place the support bracket located at the bottom of the trim front on the enclosure lip, as shown.

    NOTE: Standard trim pictured. Hinged trim support bracket pictured in Installing Low Amp Hinged Trim.

  3. Align screw holes in the trim front with the spring nuts on the enclosure lip and fasten with the 1/4-20 x 1-in. self-threading screws, included in the kit.

    NOTE: For flush-mounted applications, elevate the interior to the proper position. Refer to the information manual provided with the panelboard for more information.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?