80043-874-01

Removing and Modifying the Elevating Brackets for NQ Panelboards for MH86D9 and MH92D9

  1. Identify the end of the enclosure where the PowerPacT L circuit breaker will be installed and remove the elevating brackets on that end per the following instructions.

  2. Unscrew the nuts from the studs welded in the box; studs welded in the box should remain.

  3. Remove the elevating brackets A, and B (4). Discard A. Do not remove or modify C.

  4. Unscrew the nut from B to remove the top stud.

  5. Remove the loosened top stud. Do not remove studs that are welded in the box.

  6. Place the elevating bracket B back into place.

  7. Tighten the nuts back onto the studs welded in the box. Repeat as necessary for each stud on the remaining B elevating brackets.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?