80043-874-01

Installing NQ PowerPacT L Circuit Breaker Interior Inside the Enclosure

DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS or CSA Z462 or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Install the interior into the enclosure as instructed in NQ/NQM Panelboards and QONQ Load Centers User Guide (document number 80043-712) stated in section “Interior Mounting for Square D Brand Enclosures”.

MH86D9 and MH92D9 Enclosures

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?