80043-874-01

Removing the Studs from the Elevating Brackets for NF Panelboards for MH86D9 and MH92D9

  1. Unscrew the nuts from the studs welded in the box, for the four long elevating brackets as shown below; studs welded in the box should remain. Do not remove or modify the two small elevating brackets at each end of the box.

  2. Remove the four long elevating brackets.

  3. Unscrew the nut to remove the top stud in each elevating bracket.

  4. Remove the loosened top stud in each elevating bracket. Do not remove studs that are welded in the box.

  5. Place the elevating brackets back into place.

  6. Tighten the nuts back onto the studs welded in the box.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?