80043-874-01

Removing the Elevating Brackets for NQ Panelboards from MH62D9 to MH80D9

  1. Identify the end of the enclosure where the PowerPacT L circuit breaker will be installed and remove the elevating brackets on that end per the following instructions.

  2. Unscrew the nuts from the studs welded in the box; studs welded in the box should remain.

  3. Remove the elevating brackets A and B and discard.

NOTE: Elevating bracket C shall not be removed.

MH62D9 Enclosure

MH68D9, MH74D9, and MH80D9 Enclosures

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?