Create Base Path
The Base Path is the location in which geodatabase updates (.mdb or .gdb files) are stored and made available to the Web Service. The Web Service uses these files to create the delta file sent to the client to update a client geodatabase.
Geodatabase Replication allows for multiple replication servers. However, all replication servers must point to the same Base Path. For example, assume there are two replication servers: RS1 and RS2. The Base Path location on RS1 is D:\GDB Replication\ServerBase\. This directory must be shared (as discussed below) and RS2 must point to \\RS1\GDB Replication\ServerBase\ as its Base Path.
It is recommended that the Base Path be as close to the replication server as possible for optimal performance.
The Base Path is simply a directory structure with the appropriate sharing and permissions. This image shows a sample directory structure for a Base Path, which happens to be the ServerBase folder. You can name the Base Path anything you'd like.
Assign Directory Permissions
The Base Path must meet the following requirements:
-
The Base Path directory must be shared with the domain user and must grant Read and Write share permissions (Sharing tab).
-
The Base Path directory must grant the following permissions to all clients requiring updates: Read & Execute, List Folder Contents, Read (Security tab). This allows users to get updated information using the File Copy (UNCopy) method.
-
The Base Path directory must grant the following permissions to the domain user (Security tab): Modify, Read & Execute, List Folder Contents, Read, Write.
-
The Base Path directory must grant the permissions displayed in the image below to the domain user. To access this window, right-click the Base Path, select Properties and click the Security tab. Select the domain user and click Edit. Select the domain user and click Change Permissions, then click Edit.
While creating the Base Path directory, you may wish to include an Initial Extracts folder. This folder holds the geodatabase from which the first delta will be created (geodatabase created when following the steps in the Before You Begin topic). If you wish to maintain initial extract geodatabases for your replicas, create an Initial Extract folder. You can name this folder anything you'd like.