Configuring ArcFM Viewer for ArcGIS Engine

Configuration of ArcFM Viewer requires modification of two XML files. The ArcFM Viewer.exe.layout file is used to control Esri licensing and ArcFM Solution licensing options as well as available tools and commands. The DatabaseConnections.xml file is used to list the available databases for use with ArcFM Viewer. The individual tools (e.g., tracing, object query locator) are configured just as they would be in ArcFM .

ArcFM Trace Tools require additional model names to work with ArcFM Viewer.

IMPORTANT: Feeder Manager 2.0 and ArcFM Viewer: If you configure your data for Feeder Manager 2.0 only, you can view it in ArcFM Viewer for ArcGIS Engine. You cannot, however, edit feeder data in mobile sessions. If you do, the ArcFM Viewer display doesn’t reflect your changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?