Session Manager Database Set Up - SQL
After installing ArcFM Desktop, the following scripts are placed in C:\Program Files (x86)\Miner and Miner\ArcFM Solution\Documentation\Process Framework Enterprise\MS-SQL, and are used to create the Process Framework and Session Manager schema on a SQL Server instance:
-
AddWFMData_MSSQL.sql
-
CreatePXTables_MSSQL.sql
-
CreateSMTables_MSSQL.sql
-
CreateWFMTables_MSSQL.sql
-
GrantSMRole_MSSQL.sql
-
GrantWFMRole_MSSQL.sql
Database Set Up:
The tables required by the Process Framework engine can be placed on the same SQL instance that provides the SDE geodatabase. The tables (created by the SQL scripts) must exist under a user named PROCESS.
- Optional. Create a new database on your SQL Server instance to house the Process Framework database. An existing database can be used, but it might be easier to manage (backups, disk storage, etc.) if you create a new database dedicated to the Process Framework tables.
- Create the PROCESS user in the SQL Server instance. Remember that it is mandatory the user name is PROCESS. Grant this user access to the database discussed in step 1.
- Open the SQL Server Query Analyzer window, connecting to the database discussed in step 1 as the new PROCESS user.
- Run the CreatePxTables_MSSQL script. This script will create the tables required by the Process Framework engine.
- Run the CreateSMTables_MSSQL script. This will create the tables required by Session Manager.
-
As a DBA user in SQL Server, create a role called SM_USER.
This can either be done in a Query Analyzer window or the Enterprise
Manager. This role will be used to assign the appropriate table privileges
to users of Session Manager. The name of this role is not mandatory;
however, if you use a different name for this role you will have to
alter the SQL script in the next step. The following SQL syntax will
create a role in SQL Server:
sp_addrole SM_USER;
- With the Query Analyzer, connect to the database as the PROCESS user and Run the GrantSMRole_MSSQL script. This script grants the appropriate table privileges to the SM_USER role. Again, if you changed the role name as discussed in step 6, you’ll need to alter this script to use the name you chose.
- Grant the various existing SQL Server users access to the database discussed in step 1. Since the number of users involved in this step is probably equal to the number of users that access SDE, you’ll probably want to make a script to perform this task.
- Add the various existing SQL Server users to the SM_USER role. Since the number of users involved in this step is probably equal to the number of users that access SDE, you’ll probably want to write a script to perform this task.
- To add a workflow, use the Import/Export tab in the Process Framework Administration tool and the sample Session Manager database (SessionManager.mdb) provided with the ArcFM Solution install.
Session Manager Administration
Add each user involved in step 8 above to the Process Framework with the Users tab in the Process Framework Administration Tool. After you have imported the workflow (see Add Workflow, below), you can also use the Users tab to assign the Session Manager user roles to each user.
Add Workflow
The following steps allow you to export the workflow from the sample database provided with the ArcFM Solution installation and import that workflow into your own Process Framework database. Once imported, this workflow can be modified to meet your specific business needs.
-
Log in to SessionManager.mdb as Process.
-
Select the Import/Export tab.
-
Select the Export radio button and select the Process Framework Workflow Importer/Exporter checkbox.
-
Designate an XML file name to which the workflow will be exported.
-
Click Export and select the MMSessionManager extension.
-
Close the Process Framework Admin tool when the export is complete.
-
Log in to your Session Manager database as Process.
-
Select the Import/Export tab.
-
Select the Import radio button and browse to the XML file you just exported from the sample data.
-
Click Import.