View Only

This implementation gives mobile users the ability to view and query data in the field. The following steps walk you through setting up the enterprise as well as field machines to use Engine Mobile . Field users have access to view and query data, while Enterprise users have full ArcFM functionality as allowed by their licensing.

View Only users will not be able to send/receive sessions.

Required Licenses in the Field: ArcFM Viewer for ArcGIS Engine or ArcFM Viewer

Field Databases: Backdrop, Login (optional)

When you've finished the Engine Mobile configuration, you might want to use Geodatabase Replication to maintain updated backdrop and login databases in the field. Create a geodatabase replica for the backdrop and a directory replica to maintain the login database (if used).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?