Delete Existing Circuits

  1. Start Editing, or open a Session/Design.
  2. On the Fiber Manager toolbar, click the Circuit Manager button.
  3. In the Circuit Manager dialog, click the circuit you need to delete once to highlight it in blue. Use Ctrl and Shift to highlight multiple circuits.

  4. Click Delete.
    IMPORTANT: All edits performed by this tool are immediately saved to your session or design. In practice this means there is no undo for this tool while in your session or design. You can delete your entire session or design (or do not post it) if you do not want your circuits to be deleted in the default version of the database. 
  5. In the confirmation dialog, click Yes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?