Welcome and FAQs

Welcome to the Fiber Manager Using Guide.

Here are some tips to help you find relevant information fast:

  • Topics are organized thematically in the Table of Contents along the left-hand side. Expand topics to reveal subtopics.

  • Use the Search field to type keywords you’re looking for. The Search defaults to querying within the current guide, but it also gives you the chance to query the entire catalog of guides. Further, it allows you to filter by product, guide type, and version. Enter your search terms to get started.

    Watch this short video that walks you through how to perform a search and filter your results.

  • While reading a topic, press the down key to scroll down through the topic, press the right key to move to the next topic in the Table of Contents, and press the left key to move to the previous topic in the Table of Contents.

  • Want to send a topic to a co-worker? Click the Sharable Link tool. This copies the current topic’s URL straight to your clipboard, ready for you to paste into an email or other message.

    Want to see how the Shareable Link tool works in action? Watch this short video!

  • Is the image a little too small? Click it to open in a separate tab. It opens as large as possible.

  • Use the “Was this helpful?” feedback options to drop us a note! Your comments help us improve documentation so you can get your job done most effectively. The following video explains how the “Was this helpful?” button works.

  • Watch this video to learn more about navigating the ArcFM Solution Documentation Portal.


Frequently Asked Questions (FAQ)

What’s the user community searching for? Here are the top searches and topics visited in this guide:

Fiber Using
  1. In Connection Manager, can I filter by port number?

    1. Yes. First, set the filter field to the back or front ports. To filter to a single port, type the number (for example, 45). To filter to a range of ports, type the range within square brackets (for example, [45–55]). As an added tip, you can type an exclamation point before the range to reverse the filter and see all the ports except the ones you specify (for example, ![45–55] would display all ports except 45 through 55).

      Find out more in the View Fiber Connections topic.


  2. By default, the Fiber Trace performs the trace in all directions. How do I change it to be a directional trace where I specify which way it should go?

    1. In the Fiber User Settings, you can check Use Directional Tracing. With Directional Tracing enabled, when you perform the Fiber Trace you have an opportunity to specificy the direction before the trace initiates.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.