Open Connection Manager

Whether viewing or editing fiber connections, the procedure to open a fiber point feature in Connection Manager is the same.
  1. Click the Connection Manager button on the Fiber Manager toolbar.
  2. Use the Connection Manager  cursor to hover over a fiber feature until it highlights, then click it.

    TIP: If you select a feature that contains conflicts, the Connection Conflict Resolution tool opens.
  3. Connection Manager opens and displays the two fiber facilities that appear alphabetically first at that location.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?