Cables

When you locate or select a cable, Wavepoint displays two tabs in the left pane: Details and Fibers.

Details

This tab provides detailed information about the cable, including its start and end points and high-level attributes. You can see the start and end points labeled on the map, and you can also click the start and end points on the Details tab to view more information about them.

Fibers

The Fibers tab displays information about the strands that belong to the cable, as well as their circuit information and availability status. Wavepoint provides the ability to view multiple circuits for one fiber.

Click the link to run a trace on a fiber strand.

TIP: To locate a particular strand, either scroll through the list or use the Find tool in your web browser (Ctrl+F).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?