Print

The Print button provides a printer-friendly view of the current display in Wavepoint.

It works whether you are viewing the map, fiber connections, or inside a location.

Once on the print preview, you can still navigate and reposition the map or display prior to printing.

IMPORTANT: In order to see the Wavepoint graphics on your print (for example, the graphics in a one-line diagram), you must check the option to print the background in your browser settings.
  • Chrome: Customize and Control Google Chrome Menu > Print > More Settings > check "Background graphics"

  • Firefox: Open Application Menu > Print > More Settings > check "Print backgrounds"

  • Internet Explorer: Tools icon (not the menu) > Print > Page Setup > check "Print Background Colors and Images"

  • Edge: Settings and More Menu > Print > More Settings > check "Background graphics"

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?