Search

Located in the upper right portion of your browser, the search bar in Wavepoint is the primary way to navigate your network. You can use it in two ways:

  • Address search: You can type all or part of an address and click the Search as Address  button.

  • Search for specific features: The Search field also queries the primary display field for all fiber feature classes belonging to the layers configured for Wavepoint. The Search field refines the list of results as you type and groups the results by feature class. Clicking the fiber feature in the Search results opens detailed information and graphical views for the following feature classes:

    • Fiber optic cables

    • Circuits

    • Patch locations

    • Racks (and devices)

    • Splice points

    TIP: To the left of the search field is a Layers drop-down, which allows you to pre-filter your search for only certain kinds of fiber facilities.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?