Welcome and FAQs
Welcome to the Wavepoint Using Guide.
Here are some tips to help you find relevant information fast:
-
Topics are organized thematically in the Table of Contents along the left-hand side. Expand topics to reveal subtopics.
-
Use the Search
field to type keywords you’re
looking for. The Search queries the entire catalog of guides, and further, it allows you to filter by product, guide type, and
version. Enter your search terms to get started. -
While reading a topic, press the down key to scroll down through the topic, press the right key to move to the next topic in the Table of Contents, and press the left key to move to the previous topic in the Table of Contents.
-
Want to send a topic to a co-worker? Click the Sharable Link
tool. This copies the current topic’s URL straight to your
clipboard, ready for you to paste into an email or other message. -
Is the image a little too small? Click it to open in a separate tab. It opens as large as possible.
-
Use the, “Was this helpful?” feedback options to drop us a note! Your comments help us improve documentation so you can get your job done most effectively.
Frequently Asked Questions (FAQ)
What’s the user community searching for? Here are the top searches and topics visited in this guide:
- When viewing splice connections in the Connections tab, sometimes
I cannot see the whole buffer tube on one side or the other. Can I
move the tube?
-
Yes. On the right and left sides of the Connections tab are scroll bars. They are hidden to maximize the space to view connections. However, if you hover over the right or left side, they appear, and you can scroll up or down to re-position the buffer tube. This functionality and more is explained in the Splice Points topic.
-