Legend

On the main toolbar, the Toggle Legend button provides a list of features in the map and their symbols.

When you click the Toggle Legend  button, all of the features viewable at your current scale are listed on a Legend tab in the left pane (the following image is just an example, and your layers, names, and symbols differ depending on your map).

IMPORTANT: When the map service is published, features are set to be visible at certain scales. The Legend respects this setting and only shows features visible at your current scale. Even if none of a particular feature is currently present in your map, that feature is still listed in the Legend if it meets the scale criterion.

There are two ways to hide the legend:

  • On the Legend tab, click the X to close.

  • On the main toolbar, click the Toggle Legend  button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?