Search

Located in the upper right portion of your browser, the search bar in Wavepoint is the primary way to navigate your network. You can use it in two ways:

  • Address Search: You can type all or part of an address and click the Search as Address  button.

  • Search for Specific Features: The Search field also queries the primary display field for all fiber feature classes belonging to the layers configured for Wavepoint.

    TIP: To the left of the search field is a Layers drop-down, which allows you to pre-filter your search for only certain kinds of fiber facilities (the following image is just an example, and your layers likely differ depending on your map).



    When searching for Active Devices, Devices, and Passive Devices (all of which are related object tables), the feature to which they are related is also returned in the search results.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?