Print

The Print button provides a printer-friendly view of the current display in Wavepoint.


It works whether you are viewing the map, fiber connections in a splice, or inside a fiber location. It also prints the one-line trace diagram, if present.

Once on the print preview, you can still navigate and reposition the map or display prior to printing.

IMPORTANT: In order to see the Wavepoint graphics on your print (for example, the graphics in a one-line diagram), you must check the option to print the background in your browser settings.
  • Chrome: Customize and Control Google Chrome Menu > Print > More Settings > check "Background graphics"

  • Firefox: Open Application Menu > Print > More Settings > check "Print backgrounds"

  • Edge: Settings and More Menu > Print > More Settings > check "Background graphics"


Splice Example


Trace Example


Patch Panel Connection Report Example

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?