DUG_Iconic Connected Switch 2AX_CLP-01

About the device

The Iconic Connected Switch 2AX operates as a switch “out-of-the-box”, with no configuration needed. The switch is available with both Bluetooth and Zigbee connectivity.
  • Switch with Zigbee default mode:

    The switch can optionally be used as one device in a Wiser Hub network. To do this, the switch must be paired to the Wiser Hub via the Wiser by SE app.

  • Switch with BLE default mode:

    The switch can be paired to a mobile phone and the Wiser by SE app. In this case, the switch can be optionally configured as a delay timer/run-on timer. The switch LED indicator behaviour can also be configured, if desired.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?