DUG_Iconic Connected Switch 2AX_CLP-01

Using the device

The Control Panel allows you to switch on/off and control various settings.

On the Home page, tap All devices > Iconic Switch to access the control panel.

On the control panel page, you can see the following:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?