DUG_Iconic Connected Switch 2AX_CLP-01

Switching on/off the device manually

You can switch on/off the device manually. The device will provide power to the electrical appliance connected to it.

Short press the push button once to turn on/off the iconic switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?