DUG_Motion_Sensor_CLP–00

Using the Device

On the Home page, tap All devices > Motion Sensor to access the control panel.

On the Sensor control panel page, you can see the following:

  • Battery level (A)

  • Motion detection status (B)

  • Current lux level (C)

  • History (D)

  • Settings (E)


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?