DUG_Smoke alarm DC_CLP-00

Example of an automation

This demonstration shows you how to create an automation to get notification on your app when the smoke is detected.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name, enter the name of the automation and tap Save.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Smoke Alarm.
  4. In Select function menu tap on Smoke Alarm > Smoke Alarm (A).

  5. Tap Add task > Send Notification and select Notifications (B).

  6. Tap Next.
  7. In the Automation Settings page, tap Save.

    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
Push notification will appear on the screen when the automation is triggered. You can also tap on icon to access the notification history.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.