DUG_Smoke alarm DC_CLP-00

Interconnecting standalone devices

The standalone devices such as 755LPSAM4 and 755RFB2 can be paired with wiser smoke alarm via RF connection.
  1. Select a device as primary and paste Primary label on the device. Other standalone devices must be considered as Secondary.
  2. On the primary device, short press the Test/ Hush button 3 times in 2 s. The Standby LED turns Red for 30 s once it is in pairing mode.

  3. Depending on the secondary device, perform one of the following:
    • For 755LPSMA4 model:
      • a. Turn the switch to the ON position located at the rear side of the device, the blue LED blinks once.
      • b. While the Standby LED on the primary device is ON for 30 s, on the secondary device, press the Test/Hush button 3 times within 2 s. Network LED blinks green for 3 s.
      • c. The network LED on the secondary device turns On for an additional 3 s.
      • d. Repeat the above steps for other secondary devices


    • For 755RFB2 model:
      • a. While the Standby LED on the primary device is ON for 30 s, on the secondary device, press wireless pairing button 3 times within 2 seconds.
      • b. The LED on the secondary device blinks 3 times indicating successful interconnection.
      • c. Repeat the above steps for other secondary devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?