DUG_Smoke alarm DC_CLP-00

Resetting the device manually

Short press (< 0,5 s) the Setup/Reset button 3 times and then long press the Setup/Reset button once for >10 s to reset the device to factory default mode.
IMPORTANT: All configuration data, user data and network data are deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.