DUG_IPC_Indoor_CLP–02

About the device

The Wiser IP Camera Indoor (hereinafter referred to as IP Camera) is a Wi-Fi® operated device that is used to monitor sensitive areas of your home. You can install the IP camera in all directions, e.g. at the ceiling or just put it on a table. The IP camera can be triggered by other Wiser devices.

Advantages of using an IP camera:

  • Increases your overall security

  • High resolution recording

  • Provides 340° view of the surrounding

  • Infrared night vision for low light recording

NOTE: Users are solely responsible for adhering to applicable laws (e.g. privacy or any other relevant laws around surveillance). Users must ensure that guarantees are taken to avoid any misuse of equipment for surveillance or entirely different and unexpected purposes than intended.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.