DUG_IPC_Indoor_CLP–02

Creating an automation

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser app, you can create automations based on your needs.
Follow the steps to create an automation:
  1. On the Home page, tap the .
  2. Go to Automation > + to create an automation.
  3. Tap Edit name, enter the name of the automation (A) and tap Save.
    TIP: You can choose the cover image that best represents your automation by tapping .

  4. Tap Any condition is met to select any one of the condition type (B):
    • All conditions are met - The automation is triggered when all the conditions are met
    • Any condition is met - The automation is triggered when at least one condition is met

  5. Tap Add Condition to open the slide-up menu.
  6. In the Add Condition menu, you can do either or all of the following options (C):
    • When weather changes - Select the various weather settings
    • Schedule - Set the time and day
    • When device status changes - Select the device and it’s function
    Note: You can add one or more conditions using .

  7. Tap When device status changes > Window/Door Sensor > Open.
    NOTE: : This is an example of an automation to turn On the Auto-patrol mode when the Window/Door is Open.
  8. Tap Add task to open the slide-up menu.
  9. In the Add task menu, you can do either or all of the following options (D):
    • Run the device - Select the devices that you want to be triggered
    • Moment or Automation - Select the moment which you want to trigger or select the automation that you want to enable or disable
    • Send notification - Turn On notification for the automation
    • Delay - Set the delay time
    NOTE: You can add one or more actions using .

  10. Tap Run the device > IP Camera Indoor > Auto-patrol Switch
  11. Select On and tap Save.

  12. Tap on Effective period to set the time range for the automation. You can select any one of the following (E):
    • All-day - 24 hours
    • Daytime - From sunrise to sunset
    • Night - From sunset to sunrise
    • Custom - User defined time period

  13. Once all the actions and conditions are set, tap Save.
    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?