DUG_IPC_Indoor_CLP–02

Detection alarm setting

The motion detection function enables the IP camera to detect motion in the surveillance area and display notifications in the Wiser app.

Follow the steps to enable the motion detection:

  1. On the Home page, tap All devices > IP Camera Indoor.

  2. Tap and tap Settings > Motion Detection.

  3. Tap the toggle switch (A) to turn On the Motion Detection Alerts.

Alarm sensitivity level

Using the Wiser app, you can adjust the sensitivity level of your motion detector.

Tap Alarm sensitivity level (B) and select any one of the following levels:

– Low

– Medium

– High

NOTE: The high sensitivity level detects the slightest movement and triggers an alarm.

Motion tracking

Enabling the Motion tracking allows the IP camera to detect the motion and automatically move the camera in the direction of the motion.

Tap the toggle switch (C) to enable the Motion tracking.

NOTE: The camera will only move in left and right directions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?