D3982892

General Description

When configured with the Active or Active+ options, SureSeT switchgear includes the Substation Monitoring Device for Medium Voltage Enhanced Switchgear. This system enables monitoring and/or remote control of the switchgear as follows:

Operations

Active Option

Active+ Option

Thermal monitoring

Environmental monitoring

Circuit breaker health monitoring

Circuit breaker control

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.