D3982892

Glossary

Acronym

Full name

BMS

Building Management System

CB

Circuit Breaker

CT

Current Transformer

HMI

Human Machine Interface

IED

Intelligent Electronic Device

LV

Low Voltage

MCM

Motor Control Monitoring

MV

Medium Voltage

PLC

Programmable Logic Controller

RFID

Radio Frequency Identification

SCADA

Supervision Control And Data Acquisition

SLD

Single Line Diagram

SMD

Substation Monitoring Device

EPME

EcoStruxure Power Monitoring Expert

EPO

EcoStruxure Power Monitoring Operation

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.