D3982892

Nearby Mode Operation

A label is included with SureSeT switchgear spare parts to help speed up the connection to the SMD HMI during operation. It is recommended to place this label in a location outside the arc flash boundary, where the switchgear front panels and the status of the pilot lights are clearly visible.

Label for Nearby Mode Operation

The instructions below provide alternative procedures that may be used in case access to such label is not available or practical.

For proper operation, make sure the following actions are completed;

  • All circuit breakers are properly inserted in their compartments. Verify their position matches the information listed on the BM100 Modbus address setting label of the circuit breaker.

  • The CL110 labeled "AMB" is correctly positioned in the designated opening on its placement guide label, located in the top-right corner of the upper front door of one of the switchgear compartments.

“AMB” CL110 sensor on SureSeT switchgear

NOTE: TH110 sensors are self-powered wireless sensors that will power on when a sufficient current flows through the switchgear bus. The sensors will not respond if sufficient current is not flowing through the conductor to which they are mounted on.

Nearby Mode with Smartphones or Tablets

  1. Connect the switchgear Wi-Fi network by scanning QR code #5 on the provided label and entering the Wi-Fi network password.

    QR code #5 on Label for Nearby Mode Operation

    If the QR code is unavailable, you can manually connect to the Wi-Fi network through your device’s Wi-Fi settings. If multiple networks are in range, make sure you connect to the correct one by verifying the switchgear factory order number on the switchgear rating nameplate.

  2. Launch the EcoStruxure Power Device app.

  3. Tap on the “Systems” tab and select the applicable SMD viewer.

  4. Tap on “Connect”.

  5. Log in the SMD by entering the applicable username and password.

The device should display the SMD HMI home page.

If the device screen appears unresponsive, check that "Operation" mode is selected in the top-left corner of the screen.

Nearby screen mirroring with “Operation” mode selected

Nearby Mode with Laptops

  1. Connect to the switchgear Wi-Fi network by entering the applicable Wi-Fi network SSID and password. If multiple Wi-Fi networks are in range, connect to the proper Wi-Fi network by verifying the switchgear factory order number on the switchgear rating nameplate.

  2. Change the laptop Wi-Fi network Internet Protocol Version 4 (TCP/IPv4) settings as follows:

    • Select “Use the following IP address”.

    • Set the Address as “192.168.4.200”.

    • Set Subnet Mask as “255.255.255.0”.

    • Set Default gateway as “192.168.4.100”.

    • Click on “OK” to confirm.

  3. Open your web browser (the use of Google Chrome is recommended) and enter “http://192.168.4.105:8082/webviewer/index.html” into the web browser bar.

  4. Log in to the SMD by entering the applicable username and password.

    If your device screen appears unresponsive, make sure that "Operation" mode is selected in the top-left corner of the screen.

Nearby laptop screen mirroring with “Operation” mode selected

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.