Connection of High-Voltage Cables
Preparation of Cable Compartment
Access to cable compartment
Mount Sealing End and Cable Lug
CAUTION |
|---|
|
hazard of incorrect mounting
Failure to follow these instructions can result in injury or equipment damage.
|
Follow the below steps to mount sealing end:
-
Route the individual cables outwards through the cable compartment of the panel to enable assembly of the cable ends.
-
Cut the rubber sleeves to fit the cable diameter, and push them onto the cables (Figure 40).
-
Strip cable ends and assemble the sealing end as specified by the cable manufacturer.
Follow the below steps to mount cable lug:
-
Fasten the individual cables to the appropriate connection surfaces (Figure 46 and Figure 47). In case of two cables per phase, connect the two cables to the first connection (Figure 47).
-
Re-mount the base plates.
-
Fasten high-voltage cable to the base plates using clamping assemblies.
-
Screw-fasten the cables (1) to the earthing bar (2) of the panel.
|
1 |
Earthing bar |
2 |
High-voltage cable |

CAUTION