GEX2564100-02

Extracting the Circuit Breaker from the Panel

Coupling the Transport Trolley

Follow the below steps to couple the transport trolley to the panel

  1. Adjust rails and unlocking bar of trolley to the correct track width of the circuit breaker (refer to Transport Trolley for Circuit Breaker ).

  2. Turn lever to the left (Figure 23, 1).

    The trolley is lifted on the front.

  3. Move trolley to the panel so that the lateral guides (Figure 24, 2) are close to the panel, and turn lever (1) back to the right. The trolley is locked on the panel (3).

Figure 23
Turning Lever on Trolley to the Left

Figure 24
Locking Transport Trolley on Panel

Extracting the Circuit breaker

Follow the below steps to remove the Circuit breaker:

  1. Push unlocking bar (Figure 25, 4) forward to its stop.

    The latching of the circuit breaker in the panel is released.

  2. Pull the circuit breaker onto the trolley via the two handles (5) until it snaps in on the trolley audibly.

  3. Turn lever back to the left (6).

    The trolley is lifted on the front, and extracted from the panel.

  4. Pull trolley with the circuit breaker away from the panel (Figure 26, 7) and turn lever back to the right to lower it (8).

    Figure 25
    Coupling the Transport Trolley to Panel

    Figure 26
    Extracting the Circuit Breaker onto Trolley

  5. Now the circuit breaker can be raised by means of a crane, and deposited.

    For more information, refer to Transport of Circuit Breakers. Instructions regarding lifting and transporting trucks (EasyPact EXE).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?