GEX2564100-02

Transport Trolley for Circuit Breaker

Figure 49
Transport trolley for truck

1

M10 X 220 HEX socket flat CSK head screw

6

Bush

2

M10X250 stainless steel bolt hexagon

7

Door handle

3

CSK screw M8X85

8

Blind rivet protruding HD 6.4 mm X 11 mm C

4

Ball knob

9

VCB handling trolley base plate

5

Trolley locking plate

   

Rated volt-age Ur of the panel [kV]

Panel width [mm]

Truck

Item number of trolley

≤ 12

650/800

EasyPact EXE

EIB AE1 148-01(1)

(1) The trolley can be used for panel widths of 650 mm and 800 mm.


Adjusting the track width

Follow the steps to adjusting the track width:

  1. Release three screws on each track (Figure 49, 2).

  2. Adjust the two tracks to the appropriate panel track width and check them. Remount the six screws.

  3. Adapt position of unlocking bar (10) also to the appropriate panel (same procedure).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?