990-1000015-001

Final Installation

  1. Reinstall the three front plates to the maintenance bypass cabinet.
  2. Only for dual mains: Add the provided labels for SSIB and the diagram label on the maintenance bypass cabinet.

    Single Mains

    Dual Mains

  3. Reinstall the right side panel and the rear panel to the maintenance bypass cabinet. Install four kick plates to the maintenance bypass cabinet.
  4. Close the front door on the maintenance bypass cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?