990-1000015-001

Installation Procedure

Single Mains – Top Cable Entry

Dual Mains – Top Cable Entry

Single Mains – Bottom Cable Entry

Dual Mains – Bottom Cable Entry

NOTE: An empty cabinet should be used to route the cables in bottom cable entry system.

Single Mains – Top and Bottom Cable Entry

Dual Mains – Top and Bottom Cable Entry

  1. Follow the UPS installation manual to prepare the UPS for installation.
  2. Prepare for Installation.
  3. Connect the Power Cables.
  4. Prepare Internal Signal Cables Between MBC and UPS.
  5. Connect the Signal Cables Between the Maintenance Bypass Cabinet and the UPS.
  6. Follow the UPS installation manual and other auxiliary product installation manuals to connect relevant signal cables and external communication cables in the UPS.
  7. Final Installation.
For moving or decommissioning the maintenance bypass cabinet after installation has been completed, please see Decommission or Move the Maintenance Bypass Cabinet to a New Location.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?